<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX7: Maximum read speed on ECSPI is 23 Mbit/s? Or is it 52 Mbit/s?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Maximum-read-speed-on-ECSPI-is-23-Mbit-s-Or-is-it-52-Mbit/m-p/627064#M95181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonah&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, SPI read timing (section 4.11.1.1) says that the minimum SCLK cycle&lt;/P&gt;&lt;P&gt;read timing is 43 ns, which is 23 Mbit/s. For write 15ns. In sect. Module list datasheet&lt;/P&gt;&lt;P&gt;gives very generic overview of modules capabilities and it is necessary to check exact figures&lt;/P&gt;&lt;P&gt;in detailed module timing parameters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jan 2017 23:41:27 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-01-18T23:41:27Z</dc:date>
    <item>
      <title>i.MX7: Maximum read speed on ECSPI is 23 Mbit/s? Or is it 52 Mbit/s?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Maximum-read-speed-on-ECSPI-is-23-Mbit-s-Or-is-it-52-Mbit/m-p/627063#M95180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the modules listing of the i.MX7 datasheet[1], it says of the ECSPI peripherals: "Full-duplex enhanced Synchronous Serial Interface, with data rate up to 52 Mbit/s."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, digging into the datasheet SPI timing (section 4.11.1.1) it says that the minimum SCLK cycle timing is actually 43 ns, which is actually only 23 Mbit/s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems pretty misleading, yes?&amp;nbsp; Perhaps the datasheet should be corrected to reflect that it can only achieve 52 Mbit/sec in write-only mode, and full-duplex mode is limited to 23 Mbit/s?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or am I reading it wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2017 19:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Maximum-read-speed-on-ECSPI-is-23-Mbit-s-Or-is-it-52-Mbit/m-p/627063#M95180</guid>
      <dc:creator>skrap</dc:creator>
      <dc:date>2017-01-18T19:57:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7: Maximum read speed on ECSPI is 23 Mbit/s? Or is it 52 Mbit/s?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Maximum-read-speed-on-ECSPI-is-23-Mbit-s-Or-is-it-52-Mbit/m-p/627064#M95181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonah&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, SPI read timing (section 4.11.1.1) says that the minimum SCLK cycle&lt;/P&gt;&lt;P&gt;read timing is 43 ns, which is 23 Mbit/s. For write 15ns. In sect. Module list datasheet&lt;/P&gt;&lt;P&gt;gives very generic overview of modules capabilities and it is necessary to check exact figures&lt;/P&gt;&lt;P&gt;in detailed module timing parameters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2017 23:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Maximum-read-speed-on-ECSPI-is-23-Mbit-s-Or-is-it-52-Mbit/m-p/627064#M95181</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-18T23:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7: Maximum read speed on ECSPI is 23 Mbit/s? Or is it 52 Mbit/s?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Maximum-read-speed-on-ECSPI-is-23-Mbit-s-Or-is-it-52-Mbit/m-p/627065#M95182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;While the module list in the datasheet is very generic, it is inexcusable for it to actually contain erroneous assertions about the features&amp;nbsp;of the hardware. &amp;nbsp; Saying &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;"Full-duplex enhanced Synchronous Serial Interface" would be generic, while&amp;nbsp;&lt;SPAN&gt;"Full-duplex enhanced Synchronous Serial Interface, with data rate up to 52 Mbit/s." is fraudulent.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;We are very&amp;nbsp;disappointed, in that it is rare to find an SPI interface that can't handle the base rate of 48 Mb/s these days. &amp;nbsp;Since you can't fix your silicon, you could at least be honest about its capabilities in the documentation.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;John&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jan 2017 01:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Maximum-read-speed-on-ECSPI-is-23-Mbit-s-Or-is-it-52-Mbit/m-p/627065#M95182</guid>
      <dc:creator>wad1</dc:creator>
      <dc:date>2017-01-19T01:14:05Z</dc:date>
    </item>
  </channel>
</rss>