<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 KitKat 4.4.3 on Linux Kernel 4.1.15?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/KitKat-4-4-3-on-Linux-Kernel-4-1-15/m-p/626686#M95102</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wondering how I could run/add the newest Linux kernel &amp;nbsp;4.1.15 for Android KitKat 4.4.3 (that currently is running linux 3.10.53) on the SabreLite board? I know it should be possible, but will NXP ever release something like that, or will I have to work on this myself?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And if anyone has an interest, could you give me some tips/pointers on developing this (I want to start working on this, and &lt;EM&gt;hopefully&lt;/EM&gt; have it done by the end of the year).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jan 2017 14:42:21 GMT</pubDate>
    <dc:creator>eric_reyna</dc:creator>
    <dc:date>2017-01-18T14:42:21Z</dc:date>
    <item>
      <title>KitKat 4.4.3 on Linux Kernel 4.1.15?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/KitKat-4-4-3-on-Linux-Kernel-4-1-15/m-p/626686#M95102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wondering how I could run/add the newest Linux kernel &amp;nbsp;4.1.15 for Android KitKat 4.4.3 (that currently is running linux 3.10.53) on the SabreLite board? I know it should be possible, but will NXP ever release something like that, or will I have to work on this myself?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And if anyone has an interest, could you give me some tips/pointers on developing this (I want to start working on this, and &lt;EM&gt;hopefully&lt;/EM&gt; have it done by the end of the year).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2017 14:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/KitKat-4-4-3-on-Linux-Kernel-4-1-15/m-p/626686#M95102</guid>
      <dc:creator>eric_reyna</dc:creator>
      <dc:date>2017-01-18T14:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: KitKat 4.4.3 on Linux Kernel 4.1.15?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/KitKat-4-4-3-on-Linux-Kernel-4-1-15/m-p/626687#M95103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of Android KitKat 4.4 with Linux kernel &amp;nbsp;4.1.15, seems one can start with:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i.MX Yocto Project: How can I (quickly) modify the kernel and test it?&lt;BR /&gt;&amp;nbsp;&lt;A href="https://community.freescale.com/docs/DOC-95003"&gt;https://community.freescale.com/docs/DOC-95003&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2017 23:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/KitKat-4-4-3-on-Linux-Kernel-4-1-15/m-p/626687#M95103</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-18T23:53:44Z</dc:date>
    </item>
  </channel>
</rss>