<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question, i.MX6Q USB complaint test in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-complaint-test/m-p/626626#M95092</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My customer is trying to handle USB module of i.MX6Q-SABRE for the preparation of USB certification test.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Referring to the following community thread, they are trying to execute the memtool commands.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/383925"&gt;https://community.nxp.com/thread/383925&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When they executed the commands, i.MX6Q stopped as below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ root@imx6qsabresd:~# /unit_tests/memtool 0x2184184=0x18411205&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ Writing 32-bit value 0x18411205 t&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The environment is as below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;OS: LinuxBSP(3.14.28)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Board: i.MX6Q-SABRE&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please find the attached file for the board connection.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you have any ideas about the cause of this issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Miyamoto&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2016 05:50:14 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2016-10-12T05:50:14Z</dc:date>
    <item>
      <title>Question, i.MX6Q USB complaint test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-complaint-test/m-p/626626#M95092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My customer is trying to handle USB module of i.MX6Q-SABRE for the preparation of USB certification test.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Referring to the following community thread, they are trying to execute the memtool commands.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/383925"&gt;https://community.nxp.com/thread/383925&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When they executed the commands, i.MX6Q stopped as below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ root@imx6qsabresd:~# /unit_tests/memtool 0x2184184=0x18411205&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ Writing 32-bit value 0x18411205 t&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The environment is as below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;OS: LinuxBSP(3.14.28)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Board: i.MX6Q-SABRE&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please find the attached file for the board connection.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do you have any ideas about the cause of this issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Miyamoto&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 05:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-complaint-test/m-p/626626#M95092</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2016-10-12T05:50:14Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q USB complaint test</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-complaint-test/m-p/626627#M95093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; From the original thread&amp;nbsp;&lt;A href="https://community.nxp.com/thread/383925"&gt;https://community.nxp.com/thread/383925&lt;/A&gt;&amp;nbsp; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;"Use memtool to set the USB PHY registers Port Status &amp;amp; Control (USBC_n_PORTSC1) &lt;BR /&gt;directly to output the specified pattern, &lt;/SPAN&gt;&lt;EM style="text-decoration: underline;"&gt;&lt;SPAN class=""&gt;make sure a HS device is connected to DUT before setting, &lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;EM style="text-decoration: underline;"&gt;&lt;SPAN class=""&gt;otherwise system might crash."&lt;/SPAN&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Answer button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 07:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-complaint-test/m-p/626627#M95093</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-10-12T07:13:21Z</dc:date>
    </item>
  </channel>
</rss>