<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: HDMI Support for IMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Support-for-IMX6/m-p/625998#M94987</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ajay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is full name of board, if this is Sabre SD then&lt;/P&gt;&lt;P&gt;mfgtool2-yocto-mx-sabresd-sdcard-sd2.vbs should be used.&lt;/P&gt;&lt;P&gt;Also valid kernel boot parameter should be used, please check p.14&lt;/P&gt;&lt;P&gt;attached Linux Guide. Use "True" HDMI display with special HDMI cable, &lt;BR /&gt;not HDMI - DVI adapter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Nov 2016 10:44:58 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-11-28T10:44:58Z</dc:date>
    <item>
      <title>HDMI Support for IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Support-for-IMX6/m-p/625997#M94986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the IMX6 sabre board. I have flashed the yocto-mx-sabreauto-sdcard-sd3 image using mfgtool2. The main purpose of the board is to display a video but I am not able to get any HDMI output when connected to a screen. Also after booting up, I am getting the following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: HDMI Video is not ready!&lt;BR /&gt;imx-hdmi-audio imx-hdmi-audio: ASoC: can't open platform imx-hdmi-audio: -22&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I resolve this error?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 07:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Support-for-IMX6/m-p/625997#M94986</guid>
      <dc:creator>ajayvenkatakris</dc:creator>
      <dc:date>2016-11-28T07:45:52Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI Support for IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Support-for-IMX6/m-p/625998#M94987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ajay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is full name of board, if this is Sabre SD then&lt;/P&gt;&lt;P&gt;mfgtool2-yocto-mx-sabresd-sdcard-sd2.vbs should be used.&lt;/P&gt;&lt;P&gt;Also valid kernel boot parameter should be used, please check p.14&lt;/P&gt;&lt;P&gt;attached Linux Guide. Use "True" HDMI display with special HDMI cable, &lt;BR /&gt;not HDMI - DVI adapter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 10:44:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Support-for-IMX6/m-p/625998#M94987</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-28T10:44:58Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI Support for IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Support-for-IMX6/m-p/625999#M94988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Board name :&amp;nbsp;MX6Q-Sabreauto revA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P14 of which document should I check. Also we tried using a HDMI-VGA adapter. Would it not work that way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 11:10:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Support-for-IMX6/m-p/625999#M94988</guid>
      <dc:creator>ajayvenkatakris</dc:creator>
      <dc:date>2016-11-28T11:10:25Z</dc:date>
    </item>
  </channel>
</rss>