<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IPU Restrictions on Frame width and Height ?? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IPU-Restrictions-on-Frame-width-and-Height/m-p/625762#M94947</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Artur.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;since the MIPI-CSI2 -&amp;gt; Gasket -&amp;gt; CSI -&amp;gt; IDMAC -&amp;gt; MEM chain is quite complicated in configuration and setup. &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;If that's the case, it should not work for any resolution and as I said, some restriciton is there in code also. Why ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any restriction is there to have width and height should be in multiples of 8 and it should be dividable by 4 ?&lt;/P&gt;&lt;P&gt;These are handled in "ipu_init_channel_buffer" function "drivers/mxc/ipu3/ipu_common.c"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If still you are doubt about our register configuration settings, then can you please tell what are the registers need to check ?&lt;/P&gt;&lt;P&gt;I've modified the registers for camera based on clock, (DPHY registers), lanes count, vc settings, data format/type etc.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please help me on this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jan 2017 04:09:49 GMT</pubDate>
    <dc:creator>titusstalin</dc:creator>
    <dc:date>2017-01-27T04:09:49Z</dc:date>
    <item>
      <title>IPU Restrictions on Frame width and Height ??</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-Restrictions-on-Frame-width-and-Height/m-p/625760#M94945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I am working with MIPI camera which stream the frames in any resolution say 12x12, 800x600, 640x480, 1200x1200 etc.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm able to get the frame 1200x1200 data perfectly, but I'm not able to get the data 1204x1204 resolution.&lt;/P&gt;&lt;P&gt;What could be the problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, my driver is configured in SMFC mode (i.e IC block is not used)&lt;/P&gt;&lt;P&gt;That is "CSI &amp;lt;-&amp;gt; MEM" configuration used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any restriction is there to have width and height should be in multiples of 8 and it should be dividable by 4 ?&lt;/P&gt;&lt;P&gt;These are handled in "ipu_init_channel_buffer" function "drivers/mxc/ipu3/ipu_common.c"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please point out in reference manual if any restrictions available like that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've referred CPMEM register, in that I saw "Frame height" and "Frame width" but its not mentioned to be multiples of 8 like that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please clarify ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support so far.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Titus S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jan 2017 06:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-Restrictions-on-Frame-width-and-Height/m-p/625760#M94945</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2017-01-18T06:05:55Z</dc:date>
    </item>
    <item>
      <title>Re: IPU Restrictions on Frame width and Height ??</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-Restrictions-on-Frame-width-and-Height/m-p/625761#M94946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no restricition in frame width or height within IPU. The possible cause of the issue is some wrong interface/IPU configuration, since the MIPI-CSI2 -&amp;gt; Gasket -&amp;gt; CSI -&amp;gt; IDMAC -&amp;gt; MEM chain is quite complicated in configuration and setup. Please follow the "MIPI–CSI2 Peripheral on i.MX6 MPUs" AN5305 Application Note document to check your camera/interface/IPU configuration. The document is available on the processor's Documentation web page (check the "Application Notes" section):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fautomotive-products%2Fmicrocontrollers-and-processors%2Farm-mcus-and-mpus%2Fi.mx-application-processors%2Fi.mx-6-processors%2Fi.mx-6quad-processors-high-performance-3d-graphics-hd-video-arm-cortex-a9-core%3Ai.MX6Q%3Ftab%3DDocumentation_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/i.mx-application-processors/i.mx-6-processors/i.mx-6quad-processors-high-performance-3d-graphics-hd-video-arm-cortex-a9-core:i.MX6Q?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2017 11:23:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-Restrictions-on-Frame-width-and-Height/m-p/625761#M94946</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2017-01-26T11:23:35Z</dc:date>
    </item>
    <item>
      <title>Re: IPU Restrictions on Frame width and Height ??</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IPU-Restrictions-on-Frame-width-and-Height/m-p/625762#M94947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Artur.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;since the MIPI-CSI2 -&amp;gt; Gasket -&amp;gt; CSI -&amp;gt; IDMAC -&amp;gt; MEM chain is quite complicated in configuration and setup. &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;If that's the case, it should not work for any resolution and as I said, some restriciton is there in code also. Why ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any restriction is there to have width and height should be in multiples of 8 and it should be dividable by 4 ?&lt;/P&gt;&lt;P&gt;These are handled in "ipu_init_channel_buffer" function "drivers/mxc/ipu3/ipu_common.c"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If still you are doubt about our register configuration settings, then can you please tell what are the registers need to check ?&lt;/P&gt;&lt;P&gt;I've modified the registers for camera based on clock, (DPHY registers), lanes count, vc settings, data format/type etc.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please help me on this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2017 04:09:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IPU-Restrictions-on-Frame-width-and-Height/m-p/625762#M94947</guid>
      <dc:creator>titusstalin</dc:creator>
      <dc:date>2017-01-27T04:09:49Z</dc:date>
    </item>
  </channel>
</rss>