<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Why native build depend required in Apache2 build</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Why-native-build-depend-required-in-Apache2-build/m-p/624239#M94729</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps it uses native Apache installation to build configuration of cross-compiled Apache.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Dec 2016 02:58:04 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-12-23T02:58:04Z</dc:date>
    <item>
      <title>Why native build depend required in Apache2 build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-native-build-depend-required-in-Apache2-build/m-p/624238#M94728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to build an Apache 2.2 image and I am looking at the Apache 2.4 recipe as a basis. I see that Apache 2.4 depends on the native build of apache. can someone explain why the native build is required for the cross-compile build? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Dec 2016 15:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-native-build-depend-required-in-Apache2-build/m-p/624238#M94728</guid>
      <dc:creator>dougbailey</dc:creator>
      <dc:date>2016-12-19T15:50:40Z</dc:date>
    </item>
    <item>
      <title>Re: Why native build depend required in Apache2 build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-native-build-depend-required-in-Apache2-build/m-p/624239#M94729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhaps it uses native Apache installation to build configuration of cross-compiled Apache.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Dec 2016 02:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-native-build-depend-required-in-Apache2-build/m-p/624239#M94729</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-12-23T02:58:04Z</dc:date>
    </item>
  </channel>
</rss>