<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SPS/PPS generation using VPU/iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPS-PPS-generation-using-VPU-iMX6/m-p/623296#M94528</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We did some investigation regarding to frame rate information in i.MX6Q&lt;BR /&gt;and found that VPU can not guarantee the frame rate reported always be valid since it depend on format (or stream).&lt;BR /&gt;However you can refer to the variable frameRateRes and frameRateDiv defined in vpu_lib.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Feb 2017 08:26:31 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-02-17T08:26:31Z</dc:date>
    <item>
      <title>SPS/PPS generation using VPU/iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPS-PPS-generation-using-VPU-iMX6/m-p/623295#M94527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a simple question.&lt;/P&gt;&lt;P&gt;My colleague is designing a H.264 encoder using iMX6/VPU.&lt;/P&gt;&lt;P&gt;Although the H.264 stream is created, it seems that the frame rate information is not included in the stream.&lt;/P&gt;&lt;P&gt;For example, when we play the stream using VLC media player, it works at the default frame rate, not at the encoded frame rate.&lt;BR /&gt;I think that such information should be included in SPS or PPS.&lt;/P&gt;&lt;P&gt;Does anyone know how to include the frame rate information in H.164 stream?&lt;/P&gt;&lt;P&gt;Thanks in advance for your advice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tetsuo Maeda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 05:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPS-PPS-generation-using-VPU-iMX6/m-p/623295#M94527</guid>
      <dc:creator>tetsuomaeda</dc:creator>
      <dc:date>2017-01-17T05:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: SPS/PPS generation using VPU/iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPS-PPS-generation-using-VPU-iMX6/m-p/623296#M94528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We did some investigation regarding to frame rate information in i.MX6Q&lt;BR /&gt;and found that VPU can not guarantee the frame rate reported always be valid since it depend on format (or stream).&lt;BR /&gt;However you can refer to the variable frameRateRes and frameRateDiv defined in vpu_lib.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Feb 2017 08:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPS-PPS-generation-using-VPU-iMX6/m-p/623296#M94528</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-02-17T08:26:31Z</dc:date>
    </item>
  </channel>
</rss>