<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: using initrd or initramfs on imx28evk for temp rootfs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189924#M9429</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As for initrd , sure , the bootm command in U-Boot takes up to three arguments:&lt;/P&gt;&lt;P&gt;bootm &amp;lt;kernel uImage address&amp;gt; &amp;lt;initrd address&amp;gt; &amp;lt;FDT blob address&amp;gt;&lt;/P&gt;&lt;P&gt;So if you want your initrd to be passed to kernel , just supply the second argument.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Of course, you can also use initramfs and build the ramdisk into the kernel image if needed be. That's possible if you run 'make menuconfig' in the kernel source tree, navigate into 'General setup' -&amp;gt; 'Init RAM filesystem and RAM disk...' , check it and put path to your initramfs root dir into 'Initramfs source file(s)' . Note that if you have any /dev/ nodes in your initramfs's /dev/ , you might want to read Documentation/filesystems/ramfs-rootfs-initramfs.txt (you might want to read that anyway) section 'Populating initramfs' ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 22 Feb 2014 00:22:30 GMT</pubDate>
    <dc:creator>MarekVasut</dc:creator>
    <dc:date>2014-02-22T00:22:30Z</dc:date>
    <item>
      <title>using initrd or initramfs on imx28evk for temp rootfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189920#M9425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone used initrd or initramfs on the imx28evk for a rootfs in memory?&amp;nbsp; Or use them with u-boot?&amp;nbsp; I need the ability to do have a small temp rootfs to assist in mounting a full rootfs from a USB stick (for field upgrade purposes).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2012 21:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189920#M9425</guid>
      <dc:creator>blsousan</dc:creator>
      <dc:date>2012-09-11T21:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: using initrd or initramfs on imx28evk for temp rootfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189921#M9426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am in the same boat.. Did you make it work?. If yes, please let me know the detailed instructions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 16:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189921#M9426</guid>
      <dc:creator>Gatts</dc:creator>
      <dc:date>2012-10-29T16:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: using initrd or initramfs on imx28evk for temp rootfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189922#M9427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Bill&lt;/P&gt;&lt;P&gt;We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the &lt;/P&gt;&lt;P&gt;issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 08:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189922#M9427</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-14T08:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: using initrd or initramfs on imx28evk for temp rootfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189923#M9428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I would like to know this too. Any updates?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 22:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189923#M9428</guid>
      <dc:creator>sensaurabh</dc:creator>
      <dc:date>2014-02-20T22:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: using initrd or initramfs on imx28evk for temp rootfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189924#M9429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As for initrd , sure , the bootm command in U-Boot takes up to three arguments:&lt;/P&gt;&lt;P&gt;bootm &amp;lt;kernel uImage address&amp;gt; &amp;lt;initrd address&amp;gt; &amp;lt;FDT blob address&amp;gt;&lt;/P&gt;&lt;P&gt;So if you want your initrd to be passed to kernel , just supply the second argument.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Of course, you can also use initramfs and build the ramdisk into the kernel image if needed be. That's possible if you run 'make menuconfig' in the kernel source tree, navigate into 'General setup' -&amp;gt; 'Init RAM filesystem and RAM disk...' , check it and put path to your initramfs root dir into 'Initramfs source file(s)' . Note that if you have any /dev/ nodes in your initramfs's /dev/ , you might want to read Documentation/filesystems/ramfs-rootfs-initramfs.txt (you might want to read that anyway) section 'Populating initramfs' ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Feb 2014 00:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189924#M9429</guid>
      <dc:creator>MarekVasut</dc:creator>
      <dc:date>2014-02-22T00:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: using initrd or initramfs on imx28evk for temp rootfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189925#M9430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;It seems that someone has answered the question. I will close the discussion. If you still have question, please reopen the DI or create another DI.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 03:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/using-initrd-or-initramfs-on-imx28evk-for-temp-rootfs/m-p/189925#M9430</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-24T03:27:26Z</dc:date>
    </item>
  </channel>
</rss>