<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 How do I configure  the INT0-INT7 interrupt request of GPIO1 source?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-configure-the-INT0-INT7-interrupt-request-of-GPIO1/m-p/621839#M94264</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, everybody. I am developing with I.MX6Q sabresd based board and want to capture a GPIO interrupt from a video decoder chip. When I looked up the IMX6DORM, I found that the IRQs 98-111 are for GPIO interrupt sources and IRQs 90-97 are also for GPIO1. Can anyone tell me the differences between them? How do I configure the INT0-INT7 interrupt request?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="irq.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12261i74A8DF824A2169C2/image-size/large?v=v2&amp;amp;px=999" role="button" title="irq.png" alt="irq.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jan 2017 10:31:11 GMT</pubDate>
    <dc:creator>anguschen</dc:creator>
    <dc:date>2017-01-17T10:31:11Z</dc:date>
    <item>
      <title>How do I configure  the INT0-INT7 interrupt request of GPIO1 source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-configure-the-INT0-INT7-interrupt-request-of-GPIO1/m-p/621839#M94264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, everybody. I am developing with I.MX6Q sabresd based board and want to capture a GPIO interrupt from a video decoder chip. When I looked up the IMX6DORM, I found that the IRQs 98-111 are for GPIO interrupt sources and IRQs 90-97 are also for GPIO1. Can anyone tell me the differences between them? How do I configure the INT0-INT7 interrupt request?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="irq.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12261i74A8DF824A2169C2/image-size/large?v=v2&amp;amp;px=999" role="button" title="irq.png" alt="irq.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 10:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-configure-the-INT0-INT7-interrupt-request-of-GPIO1/m-p/621839#M94264</guid>
      <dc:creator>anguschen</dc:creator>
      <dc:date>2017-01-17T10:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: How do I configure  the INT0-INT7 interrupt request of GPIO1 source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-configure-the-INT0-INT7-interrupt-request-of-GPIO1/m-p/621840#M94265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZHOUNENG&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GPIO1 INT0 means dedicated interrupt for GPIO1(0) signal. For interrupts example&lt;/P&gt;&lt;P&gt;please refer to attached gic sdk test with description in Chapter 4&lt;BR /&gt;Configuring the GIC Driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jan 2017 23:37:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-configure-the-INT0-INT7-interrupt-request-of-GPIO1/m-p/621840#M94265</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-17T23:37:52Z</dc:date>
    </item>
    <item>
      <title>Re: How do I configure  the INT0-INT7 interrupt request of GPIO1 source?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-configure-the-INT0-INT7-interrupt-request-of-GPIO1/m-p/621841#M94266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, igorpadykov, thank you for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jan 2017 09:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-configure-the-INT0-INT7-interrupt-request-of-GPIO1/m-p/621841#M94266</guid>
      <dc:creator>anguschen</dc:creator>
      <dc:date>2017-01-20T09:43:43Z</dc:date>
    </item>
  </channel>
</rss>