<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: USB OTG2 host mode VBUS toggles continuously</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG2-host-mode-VBUS-toggles-continuously/m-p/621802#M94263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologies, it is toggling between 0 and 3.2V.&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;USB_OTG2_PWR is connected to A16 (ENET2_TX_DATA1) pin and it is operating in ALT8 mode. According to the datasheet, It should work as well when connected to ENET2_TX_DATA1 pad.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Apr 2017 15:09:35 GMT</pubDate>
    <dc:creator>prabhatkumar</dc:creator>
    <dc:date>2017-04-19T15:09:35Z</dc:date>
    <item>
      <title>USB OTG2 host mode VBUS toggles continuously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG2-host-mode-VBUS-toggles-continuously/m-p/621800#M94261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In host mode, custom board USB OTG port detects the device and the USB_OTG2_ID pin goes low&amp;nbsp;but the &lt;SPAN&gt;USB_OTG2_PWR&lt;/SPAN&gt; pin from CPU is toggling from 0V to 3.2V continuously whenever a device (flash drive) is connected to the host. I checked USB_OTG2_OC pin and there is no over current issue either.&lt;/P&gt;&lt;P&gt;Can someone please explain why USB_OTG2_PWR continuously toggles when the board is in host mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2017 22:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG2-host-mode-VBUS-toggles-continuously/m-p/621800#M94261</guid>
      <dc:creator>prabhatkumar</dc:creator>
      <dc:date>2017-04-18T22:32:23Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG2 host mode VBUS toggles continuously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG2-host-mode-VBUS-toggles-continuously/m-p/621801#M94262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prabhat&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this looks like board hardware/layout error, as&lt;BR /&gt;USB_OTG2_PWR is connected on i.MX6UL EVK (SPF-28617.PDF) &lt;BR /&gt;to GPIO_2 pad and its power domain NVCC_GPIO can not exceed&lt;BR /&gt;datasheet requirements 3.6V, defined in Table 11. Operating Ranges i.MX6UL Datasheet &lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6ULCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 03:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG2-host-mode-VBUS-toggles-continuously/m-p/621801#M94262</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-19T03:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG2 host mode VBUS toggles continuously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG2-host-mode-VBUS-toggles-continuously/m-p/621802#M94263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My apologies, it is toggling between 0 and 3.2V.&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;USB_OTG2_PWR is connected to A16 (ENET2_TX_DATA1) pin and it is operating in ALT8 mode. According to the datasheet, It should work as well when connected to ENET2_TX_DATA1 pad.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 15:09:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG2-host-mode-VBUS-toggles-continuously/m-p/621802#M94263</guid>
      <dc:creator>prabhatkumar</dc:creator>
      <dc:date>2017-04-19T15:09:35Z</dc:date>
    </item>
  </channel>
</rss>