<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What USB pins are needed to use i.MX6UL as USB device only. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/What-USB-pins-are-needed-to-use-i-MX6UL-as-USB-device-only/m-p/621794#M94257</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer have a question about i.MX6UL USB.&lt;BR /&gt;They want to confirm what function should be assing to i.MX6UL pad to use i.MX6UL as USB device only.&lt;BR /&gt;Especially, whether OC and ID pin is needed or not.&lt;BR /&gt;I think both function pins are not needed with the following reason.&lt;BR /&gt;=====&lt;BR /&gt;For OC pin:&lt;BR /&gt; Over current detection is the function for USB host, so OC pin is not needed when use i.MX6UL as device.&lt;/P&gt;&lt;P&gt;For ID pin:&lt;BR /&gt; If ID is not assigned to any pins by IOMUX, ID will be floating.&lt;BR /&gt; In this case, i.MX6UL behave as USB device.&lt;BR /&gt;=====&lt;BR /&gt;Is my understanding correct?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Nov 2016 01:36:28 GMT</pubDate>
    <dc:creator>satoshishimoda</dc:creator>
    <dc:date>2016-11-02T01:36:28Z</dc:date>
    <item>
      <title>What USB pins are needed to use i.MX6UL as USB device only.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-USB-pins-are-needed-to-use-i-MX6UL-as-USB-device-only/m-p/621794#M94257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer have a question about i.MX6UL USB.&lt;BR /&gt;They want to confirm what function should be assing to i.MX6UL pad to use i.MX6UL as USB device only.&lt;BR /&gt;Especially, whether OC and ID pin is needed or not.&lt;BR /&gt;I think both function pins are not needed with the following reason.&lt;BR /&gt;=====&lt;BR /&gt;For OC pin:&lt;BR /&gt; Over current detection is the function for USB host, so OC pin is not needed when use i.MX6UL as device.&lt;/P&gt;&lt;P&gt;For ID pin:&lt;BR /&gt; If ID is not assigned to any pins by IOMUX, ID will be floating.&lt;BR /&gt; In this case, i.MX6UL behave as USB device.&lt;BR /&gt;=====&lt;BR /&gt;Is my understanding correct?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2016 01:36:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-USB-pins-are-needed-to-use-i-MX6UL-as-USB-device-only/m-p/621794#M94257</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2016-11-02T01:36:28Z</dc:date>
    </item>
    <item>
      <title>Re: What USB pins are needed to use i.MX6UL as USB device only.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/What-USB-pins-are-needed-to-use-i-MX6UL-as-USB-device-only/m-p/621795#M94258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, your understanding is correct. Moreover, the USB controller should be configured in software so as it will operate in the Device mode only and will ignore OC and ID pins.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Nov 2016 10:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/What-USB-pins-are-needed-to-use-i-MX6UL-as-USB-device-only/m-p/621795#M94258</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-11-02T10:37:35Z</dc:date>
    </item>
  </channel>
</rss>