<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Install the Extensible SDK ERROR in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621495#M94205</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same error and figured out that l need to copy all the manifest files as well as the buildtool install shell and the generated ininative tarball to the same folder where the main&amp;nbsp;install shell script was running. Hope this helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Mar 2017 21:07:01 GMT</pubDate>
    <dc:creator>xiaoqin</dc:creator>
    <dc:date>2017-03-21T21:07:01Z</dc:date>
    <item>
      <title>Install the Extensible SDK ERROR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621493#M94203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you help me to solve this problem? &lt;SPAN&gt;There were 11 WARNING and 1 ERROR&amp;nbsp;messages shown.&lt;/SPAN&gt;&amp;nbsp;The log as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;### Shell environment set up for builds. ###&lt;/P&gt;&lt;P&gt;You can now run 'bitbake &amp;lt;target&amp;gt;'&lt;/P&gt;&lt;P&gt;Common targets are:&lt;BR /&gt; core-image-minimal&lt;BR /&gt; core-image-sato&lt;BR /&gt; meta-toolchain&lt;BR /&gt; meta-ide-support&lt;/P&gt;&lt;P&gt;You can also run generated qemu images with a command like 'runqemu qemux86'&lt;BR /&gt;Preparing SDK for fsl-image-gui...&lt;BR /&gt;Parsing recipes...WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0_1.8.1.bb: Unable to get checksum for gstreamer1.0 SRC_URI entry 0001-introspection.m4-prefix-pkgconfig-paths-with-PKG_CON.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-rtsp-server_1.8.1.bb: Unable to get checksum for gstreamer1.0-rtsp-server SRC_URI entry 0001-Don-t-hardcode-libtool-name-when-using-introspection.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-rtsp-server_1.8.1.bb: Unable to get checksum for gstreamer1.0-rtsp-server SRC_URI entry 0001-introspection.m4-prefix-pkgconfig-paths-with-PKG_CON.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-good SRC_URI entry 0001-introspection.m4-prefix-pkgconfig-paths-with-PKG_CON.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-bad SRC_URI entry 0001-introspection.m4-prefix-pkgconfig-paths-with-PKG_CON.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-bad SRC_URI entry 0001-Makefile.am-don-t-hardcode-libtool-name-when-running.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-base SRC_URI entry 0001-introspection.m4-prefix-pkgconfig-paths-with-PKG_CON.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-base SRC_URI entry 0001-Makefile.am-don-t-hardcode-libtool-name-when-running.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-base SRC_URI entry 0002-Makefile.am-prefix-calls-to-pkg-config-with-PKG_CONF.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-base SRC_URI entry 0003-riff-add-missing-include-directories-when-calling-in.patch: file could not be found&lt;BR /&gt;WARNING: /home/huangzhao/fsl-imx-fb_sdk/layers/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.8.1.bb: Unable to get checksum for gstreamer1.0-plugins-base SRC_URI entry 0004-rtsp-drop-incorrect-reference-to-gstreamer-sdp-in-Ma.patch: file could not be found&lt;BR /&gt;done.&lt;BR /&gt;Parsing of 2216 .bb files complete (0 cached, 2216 parsed). 2791 targets, 439 skipped, 5 masked, 0 errors.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;BR /&gt;ERROR: Uninative selected but not configured, please set UNINATIVE_URL&lt;/P&gt;&lt;P&gt;Summary: There were 11 WARNING messages shown.&lt;BR /&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2017 04:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621493#M94203</guid>
      <dc:creator>huangzhaocn</dc:creator>
      <dc:date>2017-02-10T04:39:57Z</dc:date>
    </item>
    <item>
      <title>Re: Install the Extensible SDK ERROR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621494#M94204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you tell me more information?&lt;/P&gt;&lt;P&gt;which BSP are you using? what is the step to reproduce the issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2017 04:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621494#M94204</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-02-13T04:24:57Z</dc:date>
    </item>
    <item>
      <title>Re: Install the Extensible SDK ERROR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621495#M94205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same error and figured out that l need to copy all the manifest files as well as the buildtool install shell and the generated ininative tarball to the same folder where the main&amp;nbsp;install shell script was running. Hope this helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Mar 2017 21:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621495#M94205</guid>
      <dc:creator>xiaoqin</dc:creator>
      <dc:date>2017-03-21T21:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: Install the Extensible SDK ERROR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621496#M94206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have same question. I am also getting same error while setting up extended sdk in yocto for nxp image. I checked all manifest files and uninative tarball are also in same folder but still getting error. Did anyone got proper solution for it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Vivek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 05:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-the-Extensible-SDK-ERROR/m-p/621496#M94206</guid>
      <dc:creator>vivekrajpara</dc:creator>
      <dc:date>2017-06-01T05:00:34Z</dc:date>
    </item>
  </channel>
</rss>