<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can the ASRC block handle input/output clock skew?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-the-ASRC-block-handle-input-output-clock-skew/m-p/620221#M94014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Danny&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ASRC internally is a micro-coded FSM, so there is always delay between input and output clocks.&lt;/P&gt;&lt;P&gt;A bit more detailed description of its work can be found in its early version description in&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/reference-manuals/DSP56720RM.pdf"&gt;http://www.nxp.com/assets/documents/data/en/reference-manuals/DSP56720RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Dec 2016 23:53:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-12-16T23:53:40Z</dc:date>
    <item>
      <title>Can the ASRC block handle input/output clock skew?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-the-ASRC-block-handle-input-output-clock-skew/m-p/620220#M94013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking into using the Asynchronous Sample Rate Converter (ASRC) in the i.MX 6 family for various audio related purposes. While reading the data sheet I found this note on available features:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Automatic accommodation to slow variations in the incoming and outgoing sampling rates.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How does this feature work? Could I set incoming and outgoing clocks to 48KHz and the ASRC block would take care of the clock skew present between these clocks (for instance, one of the clocks is running slightly faster or slower than the other)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Danny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2016 10:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-the-ASRC-block-handle-input-output-clock-skew/m-p/620220#M94013</guid>
      <dc:creator>dannysmith</dc:creator>
      <dc:date>2016-12-16T10:14:02Z</dc:date>
    </item>
    <item>
      <title>Re: Can the ASRC block handle input/output clock skew?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-the-ASRC-block-handle-input-output-clock-skew/m-p/620221#M94014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Danny&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ASRC internally is a micro-coded FSM, so there is always delay between input and output clocks.&lt;/P&gt;&lt;P&gt;A bit more detailed description of its work can be found in its early version description in&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/reference-manuals/DSP56720RM.pdf"&gt;http://www.nxp.com/assets/documents/data/en/reference-manuals/DSP56720RM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2016 23:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-the-ASRC-block-handle-input-output-clock-skew/m-p/620221#M94014</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-16T23:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: Can the ASRC block handle input/output clock skew?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-the-ASRC-block-handle-input-output-clock-skew/m-p/620222#M94015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the info! I have read through the documentation but are still not sure of how the ASRC handles small variations in the input/output clocks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lets say we have a very accurate 48KHz input clock and a less accurate output clock running at 48003Hz. What will the ASRC do in this case? upsample to 48003Hz? If so, are there any limitations to this functionality?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the clocks are both running at precise 48KHz, will the ASRC keep them in sync?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Danny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2016 10:06:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-the-ASRC-block-handle-input-output-clock-skew/m-p/620222#M94015</guid>
      <dc:creator>dannysmith</dc:creator>
      <dc:date>2016-12-20T10:06:26Z</dc:date>
    </item>
  </channel>
</rss>