<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSCM with onboard NOR Flash only</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SCM-with-onboard-NOR-Flash-only/m-p/619291#M93837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to have Linux system operational with on-board 16MB NOR flash only? All the SCM user manuals describe booting from SD card process, but I cannot find any instructions about using on-board flash only. The SCM fact sheet states that "The 16MB SPI NOR flash is sized to support the storage of uboot, Linux kernel image, and an optimized Linux OS.", so I guess it is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alexey.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 09 Oct 2016 09:01:23 GMT</pubDate>
    <dc:creator>alexeytsirlin</dc:creator>
    <dc:date>2016-10-09T09:01:23Z</dc:date>
    <item>
      <title>SCM with onboard NOR Flash only</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCM-with-onboard-NOR-Flash-only/m-p/619291#M93837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to have Linux system operational with on-board 16MB NOR flash only? All the SCM user manuals describe booting from SD card process, but I cannot find any instructions about using on-board flash only. The SCM fact sheet states that "The 16MB SPI NOR flash is sized to support the storage of uboot, Linux kernel image, and an optimized Linux OS.", so I guess it is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alexey.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Oct 2016 09:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCM-with-onboard-NOR-Flash-only/m-p/619291#M93837</guid>
      <dc:creator>alexeytsirlin</dc:creator>
      <dc:date>2016-10-09T09:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: SCM with onboard NOR Flash only</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SCM-with-onboard-NOR-Flash-only/m-p/619292#M93838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexey&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please program images with Mfg Tools using script&lt;/P&gt;&lt;P&gt;mfgtool2-yocto-mx6scm-1gb-qwks-rev2-internal-spi-nor.vbs&lt;BR /&gt;Mfg Tool&lt;BR /&gt;Updates and Patches (2)&lt;BR /&gt;SCM-i.MX 6Dual/6Quad Manufacturing Toolkit for Linux 3.14.52 Patch Release (REV 1)&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Oct 2016 23:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SCM-with-onboard-NOR-Flash-only/m-p/619292#M93838</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-09T23:21:00Z</dc:date>
    </item>
  </channel>
</rss>