<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Image into Framebuffer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Image-into-Framebuffer/m-p/618693#M93739</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use these examples regarding to output images into framebuffer:&lt;BR /&gt;&lt;A href="https://github.com/rogeriorps/ipu-examples/"&gt;https://github.com/rogeriorps/ipu-examples/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Feb 2017 08:02:39 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2017-02-14T08:02:39Z</dc:date>
    <item>
      <title>Image into Framebuffer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-into-Framebuffer/m-p/618692#M93738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;Ours is a custom board based on imx6 .We wanted to dump a image into the framebuffer,But this should be done without opening the /dev/fb0 node.This method is similar&amp;nbsp; to the boot up logo which is copied into the framebuffer base address.&lt;/P&gt;&lt;P&gt;But we are not able to find how they are copying the buffer into the framebuffer base address.Can any one help on how to do so.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 10:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-into-Framebuffer/m-p/618692#M93738</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2017-02-09T10:51:32Z</dc:date>
    </item>
    <item>
      <title>Re: Image into Framebuffer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-into-Framebuffer/m-p/618693#M93739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use these examples regarding to output images into framebuffer:&lt;BR /&gt;&lt;A href="https://github.com/rogeriorps/ipu-examples/"&gt;https://github.com/rogeriorps/ipu-examples/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2017 08:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-into-Framebuffer/m-p/618693#M93739</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-02-14T08:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: Image into Framebuffer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Image-into-Framebuffer/m-p/618694#M93740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually in this examples they seemed to open the /dev/fb0 and try to output image into framebuffer.But what i wanted is to output image into framebuffer without opening the /dev/fb0 i.e write the image buffer into the framebuffer RAM address&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2017 08:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Image-into-Framebuffer/m-p/618694#M93740</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2017-02-14T08:10:12Z</dc:date>
    </item>
  </channel>
</rss>