<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX6SDL camera format</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SDL-camera-format/m-p/618378#M93682</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an IMX6SDL with a CSI camera. &amp;nbsp;I'm confused whether or not I can use a YUV420 camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the CSI port is at least capable of receiving YUV420 data (41.5.10) but&amp;nbsp;the IPU looks like it won't accept YUV420 data (IPU_CSIx_SENS_CONF doesn't have YUV420 option, Table 38.2 has no YUV420 entry).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've *been* using a YUV422 camera with gst-imx to do the color conversion and encoding but would like to migrate away from a gStreamer application. &amp;nbsp;I figured if I could get the camera to ouput YUV420 and pipe it directly to the VPU I could skip having to implement the color conversion....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Mar 2017 16:42:30 GMT</pubDate>
    <dc:creator>chrisroed</dc:creator>
    <dc:date>2017-03-03T16:42:30Z</dc:date>
    <item>
      <title>IMX6SDL camera format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SDL-camera-format/m-p/618378#M93682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an IMX6SDL with a CSI camera. &amp;nbsp;I'm confused whether or not I can use a YUV420 camera?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the CSI port is at least capable of receiving YUV420 data (41.5.10) but&amp;nbsp;the IPU looks like it won't accept YUV420 data (IPU_CSIx_SENS_CONF doesn't have YUV420 option, Table 38.2 has no YUV420 entry).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've *been* using a YUV422 camera with gst-imx to do the color conversion and encoding but would like to migrate away from a gStreamer application. &amp;nbsp;I figured if I could get the camera to ouput YUV420 and pipe it directly to the VPU I could skip having to implement the color conversion....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 16:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SDL-camera-format/m-p/618378#M93682</guid>
      <dc:creator>chrisroed</dc:creator>
      <dc:date>2017-03-03T16:42:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6SDL camera format</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6SDL-camera-format/m-p/618379#M93683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check Table 37-2. Data Formats Supported By The Camera Port&lt;/P&gt;&lt;P&gt;i.MX6DQ Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;YUV420 is not supported, it can be processed as generic data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Mar 2017 00:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6SDL-camera-format/m-p/618379#M93683</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-03-04T00:26:30Z</dc:date>
    </item>
  </channel>
</rss>