<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How do I zero streambuffer of vpu?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-zero-streambuffer-of-vpu/m-p/618272#M93667</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VPU requires a specific size resolution.&amp;nbsp; If the size changes the VPU instance has to be reinitialized.&amp;nbsp; This is because when the instance is instantiated physical memory is allocated based on the size specified. &amp;nbsp;Please check&amp;nbsp;.MX 6Dual/6Quad VPU Application Programming Interface Linux Reference Manual / Document Number:VPU_API&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Nov 2016 16:22:42 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2016-11-09T16:22:42Z</dc:date>
    <item>
      <title>How do I zero streambuffer of vpu?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-zero-streambuffer-of-vpu/m-p/618271#M93666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If&amp;nbsp;vpu_DecGetBitstreamBuffer returned a zero space once, the following call of&amp;nbsp;vpu_DecGetBitstreamBuffer will always return zero.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 05:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-zero-streambuffer-of-vpu/m-p/618271#M93666</guid>
      <dc:creator>linzhang</dc:creator>
      <dc:date>2016-11-01T05:51:21Z</dc:date>
    </item>
    <item>
      <title>Re: How do I zero streambuffer of vpu?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-do-I-zero-streambuffer-of-vpu/m-p/618272#M93667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VPU requires a specific size resolution.&amp;nbsp; If the size changes the VPU instance has to be reinitialized.&amp;nbsp; This is because when the instance is instantiated physical memory is allocated based on the size specified. &amp;nbsp;Please check&amp;nbsp;.MX 6Dual/6Quad VPU Application Programming Interface Linux Reference Manual / Document Number:VPU_API&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Nov 2016 16:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-do-I-zero-streambuffer-of-vpu/m-p/618272#M93667</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2016-11-09T16:22:42Z</dc:date>
    </item>
  </channel>
</rss>