<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HDMI audio 1024 x 768  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-audio-1024-x-768/m-p/618065#M93649</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;目前我们的平台是 imx6d &amp;nbsp;+ linux3.14.52 分辨率需要增加 1024 x 768, 1440 x 900 等一些分辨率。&lt;/P&gt;&lt;P&gt;我参照&lt;A href="https://community.nxp.com/thread/432999"&gt;How to get 1366x768, 800x600 output over HDMI?&lt;/A&gt;&amp;nbsp; 进行了添加，HDMI 显示是可以正常显示，但是HDMI&amp;nbsp;&lt;/P&gt;&lt;P&gt;声音无法正常输出了。&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/weidong.sun"&gt;weidong.sun&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Feb 2017 10:03:02 GMT</pubDate>
    <dc:creator>ispsubb</dc:creator>
    <dc:date>2017-02-09T10:03:02Z</dc:date>
    <item>
      <title>HDMI audio 1024 x 768</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-audio-1024-x-768/m-p/618065#M93649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;目前我们的平台是 imx6d &amp;nbsp;+ linux3.14.52 分辨率需要增加 1024 x 768, 1440 x 900 等一些分辨率。&lt;/P&gt;&lt;P&gt;我参照&lt;A href="https://community.nxp.com/thread/432999"&gt;How to get 1366x768, 800x600 output over HDMI?&lt;/A&gt;&amp;nbsp; 进行了添加，HDMI 显示是可以正常显示，但是HDMI&amp;nbsp;&lt;/P&gt;&lt;P&gt;声音无法正常输出了。&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/weidong.sun"&gt;weidong.sun&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 10:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-audio-1024-x-768/m-p/618065#M93649</guid>
      <dc:creator>ispsubb</dc:creator>
      <dc:date>2017-02-09T10:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI audio 1024 x 768</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-audio-1024-x-768/m-p/618066#M93650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that i.MX6 HDMI module officially does not support 1366x768 mode.&lt;BR /&gt;Supported modes are listed in chapter 33.4.3 "Supported Video Mode" of i.MX 6Dual/6Quad Reference Manual:&lt;BR /&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However actually you can add kernel command line like 1366x768M@60 for 1366x768 mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you need to make sure that your monitor supports 1366x768 mode.&lt;BR /&gt;You can check it such way:&lt;BR /&gt;# cat /sys/class/graphics/fb0/modes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for sound please note that HDMI audio is handled in software by arm core in special way &lt;BR /&gt;that is described in section 16.2.5 of i.MX6 Linux Reference Manual.&lt;BR /&gt; &lt;BR /&gt;As workaround you can try attached SDMA patch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2017 06:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-audio-1024-x-768/m-p/618066#M93650</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-02-10T06:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI audio 1024 x 768</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-audio-1024-x-768/m-p/618067#M93651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;感谢你的回复！&lt;/P&gt;&lt;P&gt;新增加的分辨率，画面是可以正常显示的。只是HDMI 对应的声音不正常。&lt;/P&gt;&lt;P&gt;你的补丁在我使用的这个版本中，linux3.14.52 已经修复。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Feb 2017 03:48:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-audio-1024-x-768/m-p/618067#M93651</guid>
      <dc:creator>ispsubb</dc:creator>
      <dc:date>2017-02-11T03:48:50Z</dc:date>
    </item>
  </channel>
</rss>