<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Input protection for i.MX6S USB OTG in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Input-protection-for-i-MX6S-USB-OTG/m-p/617652#M93524</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="220949" data-username="markusbraitner" href="https://community.nxp.com/people/markusbraitner"&gt;Markus&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;About ESD protection:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(1) Considering CPU pin's rating, at first&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;About rating, see datasheet of i.MX6,please! all pins has been listed in it.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(2)Selecting ESD parts according to Pin's rating.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;There are 2 the most important parameters we must focus on :&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-----Reverse stand-off voltage&lt;/STRONG&gt; : At the voltage, ESD doesn't work.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-----Reverse broken down voltage&lt;/STRONG&gt; :After this voltage is exceeded, the diode is rapidly reversed and enters the conduction state.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(3)About Clamping Voltage&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;:After this voltage is exceeded, the diode will be damaged. The parameter is only related to ESD part, running environment of hardware and max &lt;SPAN&gt;surge voltage&lt;/SPAN&gt;, no relations with CPU pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;(Weidong)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Mar 2017 02:04:50 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2017-03-06T02:04:50Z</dc:date>
    <item>
      <title>Input protection for i.MX6S USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-protection-for-i-MX6S-USB-OTG/m-p/617651#M93523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got a question concerning the input protection of the i.MX6S USB OTG Interface:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I determine the clamp voltage needed for TVS diodes selection as ESD protection?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From 16115_IMX6SDLCEC.pdf, I can see from the absolute Maximum Ratings:&lt;/P&gt;&lt;P&gt;- USB VBUS =&amp;gt; 5.25V&lt;/P&gt;&lt;P&gt;- USB_OTG_DP, USB_OTG_DN =&amp;gt; -0.3 to 3.63V&lt;/P&gt;&lt;P&gt;- Vesd =&amp;gt; 2000V (HBM) / 500V (CDM)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the Saber Board schematics 27417 I can see that you used a SRV05-4 component for this reason, which has a clamp voltage of 12.5V @ 1A / 17.5V @ 5A. So how to determine the needed clamp voltage if I have to use some other component?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, how can I find some Information on the internal Input protection of the i.MX6 in general for figuring out which diodes&amp;nbsp;I need for clamping non-ESD overvoltage on the input?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 09:36:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-protection-for-i-MX6S-USB-OTG/m-p/617651#M93523</guid>
      <dc:creator>markusbraitner</dc:creator>
      <dc:date>2017-03-03T09:36:01Z</dc:date>
    </item>
    <item>
      <title>Re: Input protection for i.MX6S USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-protection-for-i-MX6S-USB-OTG/m-p/617652#M93524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="220949" data-username="markusbraitner" href="https://community.nxp.com/people/markusbraitner"&gt;Markus&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;About ESD protection:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(1) Considering CPU pin's rating, at first&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;About rating, see datasheet of i.MX6,please! all pins has been listed in it.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(2)Selecting ESD parts according to Pin's rating.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;There are 2 the most important parameters we must focus on :&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-----Reverse stand-off voltage&lt;/STRONG&gt; : At the voltage, ESD doesn't work.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-----Reverse broken down voltage&lt;/STRONG&gt; :After this voltage is exceeded, the diode is rapidly reversed and enters the conduction state.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(3)About Clamping Voltage&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;:After this voltage is exceeded, the diode will be damaged. The parameter is only related to ESD part, running environment of hardware and max &lt;SPAN&gt;surge voltage&lt;/SPAN&gt;, no relations with CPU pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;(Weidong)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 02:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-protection-for-i-MX6S-USB-OTG/m-p/617652#M93524</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-03-06T02:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: Input protection for i.MX6S USB OTG</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Input-protection-for-i-MX6S-USB-OTG/m-p/617653#M93525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wigros/Weidong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your answer! Howevery, it didn't answer my questions...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) How to determine the needed clamp voltage of the TVS Diode?&lt;/P&gt;&lt;P&gt;If the i.MX6 has an Vesd of 2000V (HBM) or&amp;nbsp;500V (CDM) (according to the data sheet), I guess I do need a TVS Diode only for higher ESD voltages, did I Interpret that Parameter correctly? By the way, is there somewhere more documentation on this datasheet Parameter?&lt;/P&gt;&lt;P&gt;As written above I have seen that for the Saber design from NXP/Freescale, a TVS Diode with a clamp voltage of 12.5V @ 1A / 17.5V @ 5A has been used, which is significantly higher than the Maximum input voltage for USB_OTG_DP and &amp;nbsp;USB_OTG_DN which is -0.3 to 3.63V. So how to find out which clamp voltage U_V is sufficient?&lt;/P&gt;&lt;P&gt;Or did I interpret the datasheet wrongly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) How can I find some Information on the internal Input protection of the i.MX6 in General?&lt;/P&gt;&lt;P&gt;Maybe this also helps for selecting the protection diodes for small constant voltages (being greater than the absolute Maximum Rating specified for the pin).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Mar 2017 14:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Input-protection-for-i-MX6S-USB-OTG/m-p/617653#M93525</guid>
      <dc:creator>markusbraitner</dc:creator>
      <dc:date>2017-03-06T14:09:20Z</dc:date>
    </item>
  </channel>
</rss>