<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How can I reduce the time between byte to byte when use spi tx ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-reduce-the-time-between-byte-to-byte-when-use-spi-tx/m-p/617335#M93481</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I reduce the time between byte to byte when use spi tx ?&lt;/P&gt;&lt;P&gt;I'm now using kernel version linux-4.1.15.The hardware is I.MX6UL-EVK board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 25 Mar 2017 14:46:49 GMT</pubDate>
    <dc:creator>浩卢</dc:creator>
    <dc:date>2017-03-25T14:46:49Z</dc:date>
    <item>
      <title>How can I reduce the time between byte to byte when use spi tx ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-reduce-the-time-between-byte-to-byte-when-use-spi-tx/m-p/617335#M93481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I reduce the time between byte to byte when use spi tx ?&lt;/P&gt;&lt;P&gt;I'm now using kernel version linux-4.1.15.The hardware is I.MX6UL-EVK board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Mar 2017 14:46:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-reduce-the-time-between-byte-to-byte-when-use-spi-tx/m-p/617335#M93481</guid>
      <dc:creator>浩卢</dc:creator>
      <dc:date>2017-03-25T14:46:49Z</dc:date>
    </item>
    <item>
      <title>Re: How can I reduce the time between byte to byte when use spi tx ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-reduce-the-time-between-byte-to-byte-when-use-spi-tx/m-p/617336#M93482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try to use bursts, please check description register&amp;nbsp; ECSPIx_CONREG field&lt;/P&gt;&lt;P&gt;BURST_LENGTH in sect.20.7.3 Control Register (ECSPIx_CONREG)&lt;/P&gt;&lt;P&gt;i.MX6UL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If possible increase clock frequency, max. is defined in sect.4.12.2 ECSPI timing parameters i.MX6UL Datasheet &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6ULCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Mar 2017 23:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-reduce-the-time-between-byte-to-byte-when-use-spi-tx/m-p/617336#M93482</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-03-26T23:29:16Z</dc:date>
    </item>
  </channel>
</rss>