<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Inter-processor communication between Linux and RTOS in imx6 sabrelite in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617202#M93467</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi saravanan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Chapter 51 Remote Processor Messaging&lt;/P&gt;&lt;P&gt;attached Linux Manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Jan 2017 00:10:29 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-01-14T00:10:29Z</dc:date>
    <item>
      <title>Inter-processor communication between Linux and RTOS in imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617201#M93466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using imx6 sabrelite board in which #Linux OS running on core0 and #RTOS on core2. My task is to establish inter-processor communication between two operating systems. My idea is to create shared memory section and allow read-write access using Software Generated Interrupts(SGI) between the cores. It would be really helpful for me if someone share their experience in this topic or suggest me some other approaches to accomplish this task.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 17:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617201#M93466</guid>
      <dc:creator>saravanankrish</dc:creator>
      <dc:date>2017-01-13T17:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: Inter-processor communication between Linux and RTOS in imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617202#M93467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi saravanan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Chapter 51 Remote Processor Messaging&lt;/P&gt;&lt;P&gt;attached Linux Manual&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jan 2017 00:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617202#M93467</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-14T00:10:29Z</dc:date>
    </item>
    <item>
      <title>Re: Inter-processor communication between Linux and RTOS in imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617203#M93468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your suggestion. i will look into the manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Jan 2017 13:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617203#M93468</guid>
      <dc:creator>saravanankrish</dc:creator>
      <dc:date>2017-01-14T13:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: Inter-processor communication between Linux and RTOS in imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617204#M93469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have gone through the documentation. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But , how can i implement the same on RTOS side? How can I send data from RTOS to Linux OS ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions from your side ? Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 15:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617204#M93469</guid>
      <dc:creator>saravanankrish</dc:creator>
      <dc:date>2017-01-16T15:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: Inter-processor communication between Linux and RTOS in imx6 sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617205#M93470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you solved this problem? I also encountered this problem. I would like to ask a question. To use SGI interrupts in both cores, do you need to register the interrupt function in both cores separately.&amp;nbsp;if this will cause interference?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 00:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Inter-processor-communication-between-Linux-and-RTOS-in-imx6/m-p/617205#M93470</guid>
      <dc:creator>wangzhimin</dc:creator>
      <dc:date>2018-05-18T00:51:40Z</dc:date>
    </item>
  </channel>
</rss>