<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestions about hotplugging for PCI-e interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616560#M93314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, All.&lt;/P&gt;&lt;P&gt;I am using a SABRE-AI board(CPU: i.MX6Q, Kernel: Linux imx6qsabrequto 3.14.28) for testing WiFi features.&lt;BR /&gt;For the test, a WiFi interface card is connected on a PCI-e slot of the board.&lt;BR /&gt;The interface card should be removed and re-inserted on the slot for another tests after the end of one single test.&lt;BR /&gt;I conducted the procedure for the above operation as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) # lscpi&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;01:00.0 Network controller: Qualcomm Atheros Device 003e (rev 32)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) # echo 1 &amp;gt; /sys/bus/pci/devices/0000\:01\:00.0/remove&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # lspci&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(3) The interface card for WiFi is removed and re-inserted on the PCI-e slot&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # lspci&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(4) # echo 1 &amp;gt; /sys/bus/pci/rescan&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;pcieport 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring&lt;BR /&gt;pci 0000:01:00.0: BAR 0: assigned [mem 0x01000000-0x011fffff 64bit]&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(5) # lspci&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;01:00.0 Network controller: Qualcomm Atheros Device 003e (rev 32)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seemed that PCI-e interface was normally updated, but our linux system stopped suddenly when uploading module(insmod) related with WiFi.&lt;BR /&gt;I think that something was wrong on (4) of the above procedure.&lt;BR /&gt;The following log was output as normal when I tried to rescan the interfaces without removing and re-inserting on the slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(4) # echo 1 &amp;gt; /sys/bus/pci/rescan&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;pci 0000:01:00.0: BAR 0: assigned [mem 0x01000000-0x011fffff 64bit]&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;After that, Uploading module completed successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Question is:&lt;BR /&gt;(1) Does SABRE-AI board using i.MX6Q CPU support hotplugging for PCI-e interface?&lt;BR /&gt;(2) What is the method for resolving the above issue if the board supports hotplugging for PCI-e interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Oct 2016 12:25:03 GMT</pubDate>
    <dc:creator>limlee</dc:creator>
    <dc:date>2016-10-07T12:25:03Z</dc:date>
    <item>
      <title>Questions about hotplugging for PCI-e interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616560#M93314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, All.&lt;/P&gt;&lt;P&gt;I am using a SABRE-AI board(CPU: i.MX6Q, Kernel: Linux imx6qsabrequto 3.14.28) for testing WiFi features.&lt;BR /&gt;For the test, a WiFi interface card is connected on a PCI-e slot of the board.&lt;BR /&gt;The interface card should be removed and re-inserted on the slot for another tests after the end of one single test.&lt;BR /&gt;I conducted the procedure for the above operation as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) # lscpi&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;01:00.0 Network controller: Qualcomm Atheros Device 003e (rev 32)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) # echo 1 &amp;gt; /sys/bus/pci/devices/0000\:01\:00.0/remove&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # lspci&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(3) The interface card for WiFi is removed and re-inserted on the PCI-e slot&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; # lspci&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(4) # echo 1 &amp;gt; /sys/bus/pci/rescan&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;pcieport 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring&lt;BR /&gt;pci 0000:01:00.0: BAR 0: assigned [mem 0x01000000-0x011fffff 64bit]&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(5) # lspci&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;BR /&gt;01:00.0 Network controller: Qualcomm Atheros Device 003e (rev 32)&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seemed that PCI-e interface was normally updated, but our linux system stopped suddenly when uploading module(insmod) related with WiFi.&lt;BR /&gt;I think that something was wrong on (4) of the above procedure.&lt;BR /&gt;The following log was output as normal when I tried to rescan the interfaces without removing and re-inserting on the slot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(4) # echo 1 &amp;gt; /sys/bus/pci/rescan&lt;BR /&gt;---------------------------------------------------------------------------------&lt;BR /&gt;pci 0000:01:00.0: BAR 0: assigned [mem 0x01000000-0x011fffff 64bit]&lt;BR /&gt;---------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;After that, Uploading module completed successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Question is:&lt;BR /&gt;(1) Does SABRE-AI board using i.MX6Q CPU support hotplugging for PCI-e interface?&lt;BR /&gt;(2) What is the method for resolving the above issue if the board supports hotplugging for PCI-e interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 12:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616560#M93314</guid>
      <dc:creator>limlee</dc:creator>
      <dc:date>2016-10-07T12:25:03Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about hotplugging for PCI-e interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616561#M93315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Donlim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to attached Release Notes Table 13. Known issues&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3046i97C3AA05082C7E2C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 23:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616561#M93315</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-07T23:33:00Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about hotplugging for PCI-e interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616562#M93316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;I understood that Hot Plug for PCI-e does not supported in i.MX 6Q SABRE-AI board.&lt;/P&gt;&lt;P&gt;Please let me know whether NXP has a workaround plan about Hot Plug or not.&lt;/P&gt;&lt;P&gt;To reboot the board is the best solution for re-plug PCI-e?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Oct 2016 01:00:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616562#M93316</guid>
      <dc:creator>limlee</dc:creator>
      <dc:date>2016-10-10T01:00:35Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about hotplugging for PCI-e interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616563#M93317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;there are no known plans, one can check some solutions on:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/thread/305355"&gt;https://community.freescale.com/thread/305355&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Oct 2016 06:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Questions-about-hotplugging-for-PCI-e-interface/m-p/616563#M93317</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-10T06:16:51Z</dc:date>
    </item>
  </channel>
</rss>