<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 System reboot caused by RCU warning</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/System-reboot-caused-by-RCU-warning/m-p/615741#M93132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My custom imx6q board&amp;nbsp; always reboot when running a long time LTP test.&lt;/P&gt;&lt;P&gt;hardware: imx6q with 1GHz,1G ddr3&lt;/P&gt;&lt;P&gt;kernel: Linux 3.0.35_4.1.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After running a long time LTP test, such as 4 hours, the system always reboot caused by RCU warning.&lt;/P&gt;&lt;P&gt;I have no idea what caused the problem, kernel bug or ddr parameter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, the ddr3 parameter is calibrated with ddr_stress_tester by &lt;SPAN class=""&gt;ourselves&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does any one can help me?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[189627.422520] ------------[ cut here ]------------&lt;BR /&gt;[189627.427279] WARNING: at kernel/rcutree_plugin.h:180 rcu_note_context_switch+0x19c/0x1f0()&lt;BR /&gt;[189627.435546] Modules linked in:&lt;BR /&gt;[189627.438733] [&amp;lt;c00464ac&amp;gt;] (unwind_backtrace+0x0/0x138) from [&amp;lt;c007d634&amp;gt;] (warn_slowpath_common+0x4c/0x64)&lt;BR /&gt;[189627.448311] [&amp;lt;c007d634&amp;gt;] (warn_slowpath_common+0x4c/0x64) from [&amp;lt;c007d668&amp;gt;] (warn_slowpath_null+0x1c/0x24)&lt;BR /&gt;[189627.458061] [&amp;lt;c007d668&amp;gt;] (warn_slowpath_null+0x1c/0x24) from [&amp;lt;c00c5bd8&amp;gt;] (rcu_note_context_switch+0x19c/0x1f0)&lt;BR /&gt;[189627.468261] [&amp;lt;c00c5bd8&amp;gt;] (rcu_note_context_switch+0x19c/0x1f0) from [&amp;lt;c04f6574&amp;gt;] (__schedule+0x64/0x940)&lt;BR /&gt;[189627.477841] [&amp;lt;c04f6574&amp;gt;] (__schedule+0x64/0x940) from [&amp;lt;c04f6f34&amp;gt;] (preempt_schedule+0x3c/0x58)&lt;BR /&gt;[189627.486640] [&amp;lt;c04f6f34&amp;gt;] (preempt_schedule+0x3c/0x58) from [&amp;lt;c0209428&amp;gt;] (do_msgrcv+0x1ac/0x388)&lt;BR /&gt;[189627.495435] [&amp;lt;c0209428&amp;gt;] (do_msgrcv+0x1ac/0x388) from [&amp;lt;c0209630&amp;gt;] (sys_msgrcv+0x2c/0x54)&lt;BR /&gt;[189627.503722] [&amp;lt;c0209630&amp;gt;] (sys_msgrcv+0x2c/0x54) from [&amp;lt;c003f880&amp;gt;] (ret_fast_syscall+0x0/0x30)&lt;BR /&gt;[189627.512339] ---[ end trace 5e09246341fe919e ]---&lt;BR /&gt;[189681.037049] init: untracked pid 5827 exited&lt;BR /&gt;[189687.896645]&amp;nbsp; P4231 P4231 P4231 P4231&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Oct 2016 06:07:40 GMT</pubDate>
    <dc:creator>Wizard_Richard</dc:creator>
    <dc:date>2016-10-31T06:07:40Z</dc:date>
    <item>
      <title>System reboot caused by RCU warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-reboot-caused-by-RCU-warning/m-p/615741#M93132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My custom imx6q board&amp;nbsp; always reboot when running a long time LTP test.&lt;/P&gt;&lt;P&gt;hardware: imx6q with 1GHz,1G ddr3&lt;/P&gt;&lt;P&gt;kernel: Linux 3.0.35_4.1.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After running a long time LTP test, such as 4 hours, the system always reboot caused by RCU warning.&lt;/P&gt;&lt;P&gt;I have no idea what caused the problem, kernel bug or ddr parameter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, the ddr3 parameter is calibrated with ddr_stress_tester by &lt;SPAN class=""&gt;ourselves&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does any one can help me?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[189627.422520] ------------[ cut here ]------------&lt;BR /&gt;[189627.427279] WARNING: at kernel/rcutree_plugin.h:180 rcu_note_context_switch+0x19c/0x1f0()&lt;BR /&gt;[189627.435546] Modules linked in:&lt;BR /&gt;[189627.438733] [&amp;lt;c00464ac&amp;gt;] (unwind_backtrace+0x0/0x138) from [&amp;lt;c007d634&amp;gt;] (warn_slowpath_common+0x4c/0x64)&lt;BR /&gt;[189627.448311] [&amp;lt;c007d634&amp;gt;] (warn_slowpath_common+0x4c/0x64) from [&amp;lt;c007d668&amp;gt;] (warn_slowpath_null+0x1c/0x24)&lt;BR /&gt;[189627.458061] [&amp;lt;c007d668&amp;gt;] (warn_slowpath_null+0x1c/0x24) from [&amp;lt;c00c5bd8&amp;gt;] (rcu_note_context_switch+0x19c/0x1f0)&lt;BR /&gt;[189627.468261] [&amp;lt;c00c5bd8&amp;gt;] (rcu_note_context_switch+0x19c/0x1f0) from [&amp;lt;c04f6574&amp;gt;] (__schedule+0x64/0x940)&lt;BR /&gt;[189627.477841] [&amp;lt;c04f6574&amp;gt;] (__schedule+0x64/0x940) from [&amp;lt;c04f6f34&amp;gt;] (preempt_schedule+0x3c/0x58)&lt;BR /&gt;[189627.486640] [&amp;lt;c04f6f34&amp;gt;] (preempt_schedule+0x3c/0x58) from [&amp;lt;c0209428&amp;gt;] (do_msgrcv+0x1ac/0x388)&lt;BR /&gt;[189627.495435] [&amp;lt;c0209428&amp;gt;] (do_msgrcv+0x1ac/0x388) from [&amp;lt;c0209630&amp;gt;] (sys_msgrcv+0x2c/0x54)&lt;BR /&gt;[189627.503722] [&amp;lt;c0209630&amp;gt;] (sys_msgrcv+0x2c/0x54) from [&amp;lt;c003f880&amp;gt;] (ret_fast_syscall+0x0/0x30)&lt;BR /&gt;[189627.512339] ---[ end trace 5e09246341fe919e ]---&lt;BR /&gt;[189681.037049] init: untracked pid 5827 exited&lt;BR /&gt;[189687.896645]&amp;nbsp; P4231 P4231 P4231 P4231&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2016 06:07:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-reboot-caused-by-RCU-warning/m-p/615741#M93132</guid>
      <dc:creator>Wizard_Richard</dc:creator>
      <dc:date>2016-10-31T06:07:40Z</dc:date>
    </item>
    <item>
      <title>Re: System reboot caused by RCU warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/System-reboot-caused-by-RCU-warning/m-p/615742#M93133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Richard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check (in particular Peter Chan patches)&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/thread/333368"&gt;https://community.freescale.com/thread/333368&lt;/A&gt;&lt;/P&gt;&lt;P&gt;shortly, recommended to implement all latest arm/gpu errata fixes&lt;/P&gt;&lt;P&gt;provided in latest BSP L4.1.15, like ARM-errata-7613, e.t.c.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/i.mx-6-processors/i.mx6qp/i.mx-6-series-software-and-development-tool-resources:IMX6_SW"&gt;i.MX 6 Series Software and Development Tool|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2016 09:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/System-reboot-caused-by-RCU-warning/m-p/615742#M93133</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-31T09:39:35Z</dc:date>
    </item>
  </channel>
</rss>