<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using library compiled for  ARM926EJ-S - MontaVista Linux 5.0 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614768#M92938</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The library, built for the ARM926EJ-S core and MontaVista Linux 5.0 is not guaranteed to work at all on the i.MX6's ARM Cortex A9 core and current Linux BSP. It would be better to get this library in source and then rebuild it with appropriate toolchain.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Oct 2016 09:45:43 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-10-31T09:45:43Z</dc:date>
    <item>
      <title>Using library compiled for  ARM926EJ-S - MontaVista Linux 5.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614767#M92937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="direction: ltr;"&gt;Hello,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;I need to use imx6 with a device (cryptomemory) which is supplied with a library which was compiled for for &amp;nbsp;ARM926EJ-S - MontaVista Linux 5.0&amp;nbsp;.&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Should it work with imx6 ?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;This is the link for the cryptomemory device:&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;A class="link-titled" href="http://www.atmel.com/tools/CRYPTOMEMORYDEVELOPMENTLIBRARY.aspx" title="http://www.atmel.com/tools/CRYPTOMEMORYDEVELOPMENTLIBRARY.aspx"&gt;CryptoMemory Development Library&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Best Regards,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Oct 2016 20:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614767#M92937</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2016-10-29T20:52:55Z</dc:date>
    </item>
    <item>
      <title>Re: Using library compiled for  ARM926EJ-S - MontaVista Linux 5.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614768#M92938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The library, built for the ARM926EJ-S core and MontaVista Linux 5.0 is not guaranteed to work at all on the i.MX6's ARM Cortex A9 core and current Linux BSP. It would be better to get this library in source and then rebuild it with appropriate toolchain.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2016 09:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614768#M92938</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-10-31T09:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: Using library compiled for  ARM926EJ-S - MontaVista Linux 5.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614769#M92939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure I can&amp;nbsp;will get the source code.&lt;/P&gt;&lt;P&gt;Is there a slight chance that the compiled library will run with imx6 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2016 12:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614769#M92939</guid>
      <dc:creator>rans</dc:creator>
      <dc:date>2016-10-31T12:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: Using library compiled for  ARM926EJ-S - MontaVista Linux 5.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614770#M92940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure. You can try it on your own risk.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Nov 2016 09:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-library-compiled-for-ARM926EJ-S-MontaVista-Linux-5-0/m-p/614770#M92940</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-11-01T09:54:22Z</dc:date>
    </item>
  </channel>
</rss>