<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 Linux: Is there a method for detecting temperature grade of part? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614472#M92899</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We've been working with a consumer grade i.MX6s.&lt;/P&gt;&lt;P&gt;We decided that the consumer grade part doesn't meet our temperature requirement so we're going to switch to the automotive grade part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, is there a method for detecting the temperature grade of the part through software?&lt;/P&gt;&lt;P&gt;I want to change my thermal trip points in my rc.local file if the software detects that it's running on an automotive grade part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;-Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Oct 2016 16:14:07 GMT</pubDate>
    <dc:creator>grim</dc:creator>
    <dc:date>2016-10-07T16:14:07Z</dc:date>
    <item>
      <title>i.MX6 Linux: Is there a method for detecting temperature grade of part?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614472#M92899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We've been working with a consumer grade i.MX6s.&lt;/P&gt;&lt;P&gt;We decided that the consumer grade part doesn't meet our temperature requirement so we're going to switch to the automotive grade part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, is there a method for detecting the temperature grade of the part through software?&lt;/P&gt;&lt;P&gt;I want to change my thermal trip points in my rc.local file if the software detects that it's running on an automotive grade part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;-Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 16:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614472#M92899</guid>
      <dc:creator>grim</dc:creator>
      <dc:date>2016-10-07T16:14:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Linux: Is there a method for detecting temperature grade of part?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614473#M92900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check description of fuse SPEED_GRADING&lt;/P&gt;&lt;P&gt;in Table 5-10. Fusemap Descriptions i.MX6D Reference Manual&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX6DQRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Linux checks it and automatically sets correct operating points of cpufreq, thermal&lt;/P&gt;&lt;P&gt;drivers, one can look at attached Linux Manual starting from Chapter 23.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 23:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614473#M92900</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-07T23:45:10Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Linux: Is there a method for detecting temperature grade of part?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614474#M92901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your attention to this, Igor.&lt;/P&gt;&lt;P&gt;I just want to clarify, I am using an i.MX6S. I'm not seeing the same "SPEED_GRADING" fusemap described in any of the tables in the IMX6SDLRM document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found this discussion&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/331248"&gt;https://community.nxp.com/thread/331248&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it wasn't clear to me if it's accurate to say that the SPEED_GRADING can be detected in an i.MX6S or not and if the documentation you provided pertains to the i.MX6S.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you again.&lt;/P&gt;&lt;P&gt;-Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Oct 2016 18:08:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614474#M92901</guid>
      <dc:creator>grim</dc:creator>
      <dc:date>2016-10-10T18:08:50Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Linux: Is there a method for detecting temperature grade of part?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614475#M92902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fuse location and bit registers are the same for S/DL as for the D/Q devices,&lt;/P&gt;&lt;P&gt;0x440[17:16] fuse SPEED_GRADING&lt;BR /&gt;part speed grading:&lt;BR /&gt;00 – 800 MHz&lt;BR /&gt;01 -&amp;nbsp; Reserved&lt;BR /&gt;10&amp;nbsp; - 1.0 GHz&lt;BR /&gt;11 - Reserved&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2016 00:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614475#M92902</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-11T00:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 Linux: Is there a method for detecting temperature grade of part?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614476#M92903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Oct 2016 11:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-Linux-Is-there-a-method-for-detecting-temperature-grade-of/m-p/614476#M92903</guid>
      <dc:creator>grim</dc:creator>
      <dc:date>2016-10-11T11:46:27Z</dc:date>
    </item>
  </channel>
</rss>