<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is it possible to interface two displays with MIPI interface and Two Cameras with MIPI CSI at the same time? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface-and/m-p/614360#M92888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I want to interface two displays using MIPI interface with i.MX6 Solo and these displays should work at a time with different output.Also the same with the cameras.&lt;/P&gt;&lt;P&gt;I read the i.MX6 solo reference manual but I didn't find any clue(or it may be I didn't understand) . Is this possible with i.MX6 solo?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Shree&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Apr 2017 05:42:27 GMT</pubDate>
    <dc:creator>shree97</dc:creator>
    <dc:date>2017-04-17T05:42:27Z</dc:date>
    <item>
      <title>Is it possible to interface two displays with MIPI interface and Two Cameras with MIPI CSI at the same time?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface-and/m-p/614360#M92888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I want to interface two displays using MIPI interface with i.MX6 Solo and these displays should work at a time with different output.Also the same with the cameras.&lt;/P&gt;&lt;P&gt;I read the i.MX6 solo reference manual but I didn't find any clue(or it may be I didn't understand) . Is this possible with i.MX6 solo?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Shree&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 05:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface-and/m-p/614360#M92888</guid>
      <dc:creator>shree97</dc:creator>
      <dc:date>2017-04-17T05:42:27Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to interface two displays with MIPI interface and Two Cameras with MIPI CSI at the same time?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface-and/m-p/614361#M92889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; As for multiple cameras support, please use the following :&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328548"&gt;iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;For 4xMIPI case, the four cameras should be combined (using external circuit) on the single &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;MIPI CSI2 interface, and each camera data should be transferred on a MIPI virtual channel.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; For MIPI DSI - the source of MIPI DSI is one IPU DI, so there is only one group of display timing &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;input to MIPI DSI. No several displays support.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 07:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface-and/m-p/614361#M92889</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-04-17T07:03:20Z</dc:date>
    </item>
  </channel>
</rss>