<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック[iMX6 SABRE AI] Power Adapter Specification Requirement.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-Power-Adapter-Specification-Requirement/m-p/614055#M92832</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running into a problem with iMX6 SABRE AI Sdcard with Android 5.0.2_r1 BSP build. After programed the images into the SD card and adjust the SW3, I was able to booting up but failed once the kernel executing init. The demo systrem just keeps&amp;nbsp; rebooting and I guess it might be causes by the wrong power adapter. Since I could not find these information&amp;nbsp; anywhere, could someone suggest me the ourput voltage and current of the power adapter for me. I was also using HDMI display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Justin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2016 02:15:45 GMT</pubDate>
    <dc:creator>justinfu</dc:creator>
    <dc:date>2016-11-22T02:15:45Z</dc:date>
    <item>
      <title>[iMX6 SABRE AI] Power Adapter Specification Requirement.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-Power-Adapter-Specification-Requirement/m-p/614055#M92832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running into a problem with iMX6 SABRE AI Sdcard with Android 5.0.2_r1 BSP build. After programed the images into the SD card and adjust the SW3, I was able to booting up but failed once the kernel executing init. The demo systrem just keeps&amp;nbsp; rebooting and I guess it might be causes by the wrong power adapter. Since I could not find these information&amp;nbsp; anywhere, could someone suggest me the ourput voltage and current of the power adapter for me. I was also using HDMI display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Justin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 02:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-SABRE-AI-Power-Adapter-Specification-Requirement/m-p/614055#M92832</guid>
      <dc:creator>justinfu</dc:creator>
      <dc:date>2016-11-22T02:15:45Z</dc:date>
    </item>
  </channel>
</rss>