<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Qt5 library in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613916#M92805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear friends,&lt;/P&gt;&lt;P&gt;i wanted to run qt app on ms6sabresd. i wrote a helloworld (console app) im my PC and cross-compiled it for imx6sx&lt;/P&gt;&lt;P&gt;when i attempt to run the app om the target. it says "libQt5core.so.5 not found" &amp;nbsp;also i guess it will be the same if i use widget. the embedded target is connect to my PC through NFS and the rootfs is on PC.&lt;/P&gt;&lt;P&gt;do i need new rootfs? or should i some how install library for qt on it?&lt;/P&gt;&lt;P&gt;do i need to use yocto to build rootfs? if yes which image should i use? (i work with fsl-community-bsp)&lt;/P&gt;&lt;P&gt;thank you all in advanced&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Apr 2017 05:07:36 GMT</pubDate>
    <dc:creator>adelantesey</dc:creator>
    <dc:date>2017-04-17T05:07:36Z</dc:date>
    <item>
      <title>Qt5 library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613916#M92805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear friends,&lt;/P&gt;&lt;P&gt;i wanted to run qt app on ms6sabresd. i wrote a helloworld (console app) im my PC and cross-compiled it for imx6sx&lt;/P&gt;&lt;P&gt;when i attempt to run the app om the target. it says "libQt5core.so.5 not found" &amp;nbsp;also i guess it will be the same if i use widget. the embedded target is connect to my PC through NFS and the rootfs is on PC.&lt;/P&gt;&lt;P&gt;do i need new rootfs? or should i some how install library for qt on it?&lt;/P&gt;&lt;P&gt;do i need to use yocto to build rootfs? if yes which image should i use? (i work with fsl-community-bsp)&lt;/P&gt;&lt;P&gt;thank you all in advanced&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 05:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613916#M92805</guid>
      <dc:creator>adelantesey</dc:creator>
      <dc:date>2017-04-17T05:07:36Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613917#M92806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what image do you build? let me reminder, you should build fsl-image-qt5 which includes qt5.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 08:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613917#M92806</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-04-17T08:45:48Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613918#M92807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks, but this image is not in fsl-community-bsp (it says : nothing provides fsl-image-qt5)&lt;/P&gt;&lt;P&gt;is there a way to skip bitbaking everything from the start? i mean is it possible to install the qt lib on the existing rootfs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 09:22:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613918#M92807</guid>
      <dc:creator>adelantesey</dc:creator>
      <dc:date>2017-04-17T09:22:48Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 library</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613919#M92808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can build the qt on imx6q, pls refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94066"&gt;https://community.nxp.com/docs/DOC-94066&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2017 09:08:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-library/m-p/613919#M92808</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2017-04-18T09:08:54Z</dc:date>
    </item>
  </channel>
</rss>