<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Mac to Mac communication in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613788#M92770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;We are using imx6qp controller in our project and also an ethernet switch (KSZ8795) which is having 1 mac(RGMII) and 4 phy ports.&lt;/P&gt;&lt;P&gt;The switch is connected to imx6qp in RGMII, i.e Mac to Mac and this swich is configurable with SPI and we are not using MDIO bus for configuration of switch.&lt;/P&gt;&lt;P&gt;My query is, in linux switch driver,&lt;/P&gt;&lt;P&gt;i. do i need to create PHY instance and connect to phy layer?&lt;/P&gt;&lt;P&gt;ii. do i need to create MDIO bus instance and register to bus? since i am using SPI to configure the switch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prasad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Sep 2016 14:36:44 GMT</pubDate>
    <dc:creator>prasadamjala</dc:creator>
    <dc:date>2016-09-13T14:36:44Z</dc:date>
    <item>
      <title>Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613788#M92770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;We are using imx6qp controller in our project and also an ethernet switch (KSZ8795) which is having 1 mac(RGMII) and 4 phy ports.&lt;/P&gt;&lt;P&gt;The switch is connected to imx6qp in RGMII, i.e Mac to Mac and this swich is configurable with SPI and we are not using MDIO bus for configuration of switch.&lt;/P&gt;&lt;P&gt;My query is, in linux switch driver,&lt;/P&gt;&lt;P&gt;i. do i need to create PHY instance and connect to phy layer?&lt;/P&gt;&lt;P&gt;ii. do i need to create MDIO bus instance and register to bus? since i am using SPI to configure the switch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prasad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 14:36:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613788#M92770</guid>
      <dc:creator>prasadamjala</dc:creator>
      <dc:date>2016-09-13T14:36:44Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613789#M92771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;It looks like that this switch should be used in MAC-to-MAC connection.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Set "&lt;SPAN style="background: white;"&gt;fixed-link" in .dts file for this switch. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Use additional SPI application for configuring of this switch. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 06:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613789#M92771</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-09-14T06:10:08Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613790#M92772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prasad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were you able to complete this? I am also using the ksz8795. The spi-ksz8795 driver provided by microchip is up and running and I can communicate via SPI. I am stuck at the point where the Fast Ethernet Controller Driver (FEC) can attach to the ksz8795 driver. I am unable to ping the switch.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Nov 2016 22:45:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613790#M92772</guid>
      <dc:creator>aliismail</dc:creator>
      <dc:date>2016-11-09T22:45:11Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613791#M92773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Turns out we had a hardware issue! Our RX clock was connected incorrectly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 18:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613791#M92773</guid>
      <dc:creator>aliismail</dc:creator>
      <dc:date>2016-11-15T18:41:32Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613792#M92774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;I'm using the KSZ8795 Ethernet Switch with RGMII.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I couldn't find the reference schematics.&lt;/P&gt;&lt;P&gt;Could you share the reference RGMII Interface between i.MX6 and KSZ8795 RGMII if you have?&lt;/P&gt;&lt;P&gt;It's very helpful to me if I can have it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Eric.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 08:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613792#M92774</guid>
      <dc:creator>eric_kang1</dc:creator>
      <dc:date>2017-03-03T08:11:53Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613793#M92775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好，请问你的KSZ8795已经通讯正常了吗？不知道能否指点一二，我现在也在调试这个芯片。我的SPI接口也通讯正常了，已经读出了设备ID。硬件连接采用的是RGMII接口和KSZ8795对接，SPI接口用来初始化KSZ8795，并没有使用到MDIO。我现在遇到的问题就是IMX6的fec_main.c并不能正常生成eth0的网卡设备。。。我对使用KSZ8795的理解是，现在采用这种方式连接，是否接下来要改写IMX6的fec_mian.c驱动，让他强制性认为外部有PHY，从而建立eth0设备，发出RGMII信号？？？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Jun 2018 16:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613793#M92775</guid>
      <dc:creator>suifengrumeng</dc:creator>
      <dc:date>2018-06-02T16:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613794#M92776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好，我们最近在使用ksz8895和8795 没太大区别。你们现在用的内核版本是多少？我目前跟microchip技术沟通的情况是，如果你们只是连通不用vlan等其他功能的话，可以不用spi驱动。所以首先可以不用spi驱动，先在dtsi配置好，ping通设备。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 02:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613794#M92776</guid>
      <dc:creator>zhangzhencai</dc:creator>
      <dc:date>2018-06-05T02:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613795#M92777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;恩，这种说法我在朋友那也听到了，他也是在&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;microchip技术支持那边听说的。我现在是配置了SPI驱动，那我不用SPI驱动试下吧，QQ：541237941，可以沟通下，这里审批太慢了。。。&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 15:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613795#M92777</guid>
      <dc:creator>suifengrumeng</dc:creator>
      <dc:date>2018-06-05T15:41:33Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613796#M92778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;不好意思最近比较忙没有上论坛，好的 我加你qq。不过我们开发板改版要用ksz8895 和ksz8863，现在实物还没出来，提供的建议也是很有限。我觉得你们应该找一下nxp这边的支持。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2018 10:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613796#M92778</guid>
      <dc:creator>zhangzhencai</dc:creator>
      <dc:date>2018-06-08T10:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613797#M92779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;兄弟，遇到了同样的问题，方便加下好友交流下吗。我的QQ是：164971887. &amp;nbsp; 谢谢！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 15:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613797#M92779</guid>
      <dc:creator>wqx0x</dc:creator>
      <dc:date>2019-01-14T15:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: Mac to Mac communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613798#M92780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;好的，我加你。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;zhangzhencai@transengines.com &lt;/P&gt;&lt;P&gt;上海吉盛网络技术有限公司&lt;/P&gt;&lt;P&gt;Add:中国上海漕宝路51号2楼213室&lt;/P&gt;&lt;P&gt;Phone: 021-64088876-621&lt;/P&gt;&lt;P&gt;FAX: 021-64826320&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 05:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Mac-to-Mac-communication/m-p/613798#M92780</guid>
      <dc:creator>zhangzhencai</dc:creator>
      <dc:date>2019-01-15T05:12:22Z</dc:date>
    </item>
  </channel>
</rss>