<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックhead for MC34708</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/head-for-MC34708/m-p/188904#M9248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had started software development on a custom iMX53/MC34708 based board (hardware is right in front of me) assuming that the latest head (tag rel_imx_2.6.38_11.09.01) from opensource.freescale.com/git/linux-2.6-imx.git was the actual latest. However, it appears that this doesn't include support for the MC34708 (or QSB v2) at all.&lt;/P&gt;&lt;P&gt;I did notice that MC34708 code exists back in tag rel_imx_2.6.35_11.05.01, although for some reason or other it doesn't produce uImages in quite the same format or something and aren't bootable (in the same way as newer versions at least). Maybe I was doing something simple wrong with that but I didn't really want to pursue an older branch.&lt;/P&gt;&lt;P&gt;Anyway, this was a few days before the L2.6.35_11.09.01_ER package for QSBv2 was uploaded to Freescale's website. The version of the kernel in that package does work and supports everything OK as far as I can tell so far, but just doesn't seem to match any of the opensource git branches - it's some kind of cherry picked version or a branch that isn't listed. The non-QSBv2 11.09.01 zip package might match rel_imx_2.6.38_11.09.01 but I don't want to download another GB to check.&lt;/P&gt;&lt;P&gt;Since we're working with git for control here anyway, it seems a bit inelegant to not just work directly from a properly cloned repo (i.e. from the giant base+patch pile updated every few months). Also I'm not sure if rebasing to a future version will be quite so nice if I don't have a full history (I see linaro is up to 3.x?), for inevitable support of some bleeding edge driver.&lt;/P&gt;&lt;P&gt;Am I missing something or should I just hassle Freescale to update the public repo?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2011 23:17:27 GMT</pubDate>
    <dc:creator>jpw</dc:creator>
    <dc:date>2011-11-22T23:17:27Z</dc:date>
    <item>
      <title>head for MC34708</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/head-for-MC34708/m-p/188904#M9248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had started software development on a custom iMX53/MC34708 based board (hardware is right in front of me) assuming that the latest head (tag rel_imx_2.6.38_11.09.01) from opensource.freescale.com/git/linux-2.6-imx.git was the actual latest. However, it appears that this doesn't include support for the MC34708 (or QSB v2) at all.&lt;/P&gt;&lt;P&gt;I did notice that MC34708 code exists back in tag rel_imx_2.6.35_11.05.01, although for some reason or other it doesn't produce uImages in quite the same format or something and aren't bootable (in the same way as newer versions at least). Maybe I was doing something simple wrong with that but I didn't really want to pursue an older branch.&lt;/P&gt;&lt;P&gt;Anyway, this was a few days before the L2.6.35_11.09.01_ER package for QSBv2 was uploaded to Freescale's website. The version of the kernel in that package does work and supports everything OK as far as I can tell so far, but just doesn't seem to match any of the opensource git branches - it's some kind of cherry picked version or a branch that isn't listed. The non-QSBv2 11.09.01 zip package might match rel_imx_2.6.38_11.09.01 but I don't want to download another GB to check.&lt;/P&gt;&lt;P&gt;Since we're working with git for control here anyway, it seems a bit inelegant to not just work directly from a properly cloned repo (i.e. from the giant base+patch pile updated every few months). Also I'm not sure if rebasing to a future version will be quite so nice if I don't have a full history (I see linaro is up to 3.x?), for inevitable support of some bleeding edge driver.&lt;/P&gt;&lt;P&gt;Am I missing something or should I just hassle Freescale to update the public repo?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2011 23:17:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/head-for-MC34708/m-p/188904#M9248</guid>
      <dc:creator>jpw</dc:creator>
      <dc:date>2011-11-22T23:17:27Z</dc:date>
    </item>
  </channel>
</rss>