<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PF0200 interrupt handler in Yocto 3.10 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-interrupt-handler-in-Yocto-3-10/m-p/612383#M92455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi DAVE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;INTB interrupt could be used as fault event, like pmic overheating or&lt;/P&gt;&lt;P&gt;overcurrent described in Table 100. Interrupt, Mask and Sense Bits&lt;/P&gt;&lt;P&gt;MMPF0200 Datasheet &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Seems currently this interrupt is not used in linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Oct 2016 23:26:47 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-10-06T23:26:47Z</dc:date>
    <item>
      <title>PF0200 interrupt handler in Yocto 3.10</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-interrupt-handler-in-Yocto-3-10/m-p/612382#M92454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do I use/handle the INTB interrupt from the PF0200 PMIC in Yocto 3.10?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2016 13:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-interrupt-handler-in-Yocto-3-10/m-p/612382#M92454</guid>
      <dc:creator>davesimonson</dc:creator>
      <dc:date>2016-10-06T13:51:03Z</dc:date>
    </item>
    <item>
      <title>Re: PF0200 interrupt handler in Yocto 3.10</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-interrupt-handler-in-Yocto-3-10/m-p/612383#M92455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi DAVE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;INTB interrupt could be used as fault event, like pmic overheating or&lt;/P&gt;&lt;P&gt;overcurrent described in Table 100. Interrupt, Mask and Sense Bits&lt;/P&gt;&lt;P&gt;MMPF0200 Datasheet &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf"&gt;http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0200.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Seems currently this interrupt is not used in linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2016 23:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-interrupt-handler-in-Yocto-3-10/m-p/612383#M92455</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-06T23:26:47Z</dc:date>
    </item>
  </channel>
</rss>