<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mfgtool (android) for emmc in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-android-for-emmc/m-p/611914#M92393</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi luke&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it working with sd card and default images&lt;BR /&gt;&lt;A href="http://www.nxp.com/webapp/Download?colCode=IMX_KK4.4.3_MFG_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=IMX_KK4.4.3_MFG_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also one can check signal EPDC_PWRCOM (USBOTG1_ID)&amp;nbsp; on i.MX6SL EVK &lt;BR /&gt;schematic spf-27452 is high or floating and if processor VDD_USB_CAP is powered.&lt;/P&gt;&lt;P&gt;Just for test one can try with another board or with additional usb hub.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Apr 2017 23:21:52 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-04-16T23:21:52Z</dc:date>
    <item>
      <title>mfgtool (android) for emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-android-for-emmc/m-p/611913#M92392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are developing our android project base on&amp;nbsp;&amp;nbsp;imx6sl 4.4.3&amp;nbsp;platform.&amp;nbsp;&lt;/P&gt;&lt;P&gt;in our project, we use emmc instead of sdcard in imx6sl demo board.and use mfgtool for the firmware updating.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the mfgtool stop at "No Device connected" after "start" pressed.&lt;/P&gt;&lt;P&gt;if I disconnect the usb, then connect the usb ; the PC will recognize the device, the console&amp;nbsp;will print the log&amp;nbsp;&amp;nbsp;"g_mass_storage gadget:high-speed config #1:Linux File-Backed Storage", and the mfgtool will start the firmware updating.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for the firmware updating processing, everything works fine except I have to re-connect the usb for each updating.&lt;/P&gt;&lt;P&gt;do you have any idea about how to fix this re-connect usb issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Apr 2017 04:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-android-for-emmc/m-p/611913#M92392</guid>
      <dc:creator>lukeli</dc:creator>
      <dc:date>2017-04-15T04:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool (android) for emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-android-for-emmc/m-p/611914#M92393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi luke&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is it working with sd card and default images&lt;BR /&gt;&lt;A href="http://www.nxp.com/webapp/Download?colCode=IMX_KK4.4.3_MFG_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product"&gt;http://www.nxp.com/webapp/Download?colCode=IMX_KK4.4.3_MFG_TOOL&amp;amp;appType=license&amp;amp;location=null&amp;amp;Parent_nodeId=1337699481071706174845&amp;amp;Parent_pageType=product&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also one can check signal EPDC_PWRCOM (USBOTG1_ID)&amp;nbsp; on i.MX6SL EVK &lt;BR /&gt;schematic spf-27452 is high or floating and if processor VDD_USB_CAP is powered.&lt;/P&gt;&lt;P&gt;Just for test one can try with another board or with additional usb hub.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Apr 2017 23:21:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-android-for-emmc/m-p/611914#M92393</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-04-16T23:21:52Z</dc:date>
    </item>
  </channel>
</rss>