<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Is Write Leveling required for all DDR3?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-Write-Leveling-required-for-all-DDR3/m-p/611608#M92334</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vic&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;finding optimal timings with write calibration improves&lt;/P&gt;&lt;P&gt;system stability, in general one can use ddr settings for&lt;/P&gt;&lt;P&gt;nxp reference boards with similar configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2016 23:36:05 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-11-22T23:36:05Z</dc:date>
    <item>
      <title>Is Write Leveling required for all DDR3?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-Write-Leveling-required-for-all-DDR3/m-p/611607#M92333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So we have a development project that used iMX6 and 4 modules of DDR3. There is a note on the schematic about bit swapping &amp;nbsp;on low order bit of each byte must reside at bit 0 of the byte. Somehow, this was not followed by our third party PCB layout designer and he designed it as below. The PCB is now manufactured and being assembled at our SMT line. With the bit swapping issue, obviously we can not do write calibration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, does write calibration always required for DDR3? Can we still use the finished PCB to continue with our development?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8628i7194EEA73F98734C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 15:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-Write-Leveling-required-for-all-DDR3/m-p/611607#M92333</guid>
      <dc:creator>victorsv1978</dc:creator>
      <dc:date>2016-11-22T15:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: Is Write Leveling required for all DDR3?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-Write-Leveling-required-for-all-DDR3/m-p/611608#M92334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vic&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;finding optimal timings with write calibration improves&lt;/P&gt;&lt;P&gt;system stability, in general one can use ddr settings for&lt;/P&gt;&lt;P&gt;nxp reference boards with similar configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 23:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-Write-Leveling-required-for-all-DDR3/m-p/611608#M92334</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-22T23:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: Is Write Leveling required for all DDR3?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-Write-Leveling-required-for-all-DDR3/m-p/611609#M92335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That you for your answer, that clarifies a lot. However, how can we use DDR settings from the reference boards and apply it to our design? Do you have any documentation how is it done?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Vic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Nov 2016 14:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-Write-Leveling-required-for-all-DDR3/m-p/611609#M92335</guid>
      <dc:creator>victorsv1978</dc:creator>
      <dc:date>2016-11-23T14:13:23Z</dc:date>
    </item>
  </channel>
</rss>