<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx283 spidev in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx283-spidev/m-p/611245#M92265</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with imx283 and linux-2.6.35.3&lt;/P&gt;&lt;P&gt;Does the spidev support 16-bits transfer per word ?&lt;/P&gt;&lt;P&gt;I am able to use 8-bits per word.&lt;/P&gt;&lt;P&gt;But, if i set the bits to 16. Getting following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Output:&lt;/P&gt;&lt;P&gt;spidev spi1.0: mxs_spi_setup_transfer, unsupported bits_per_word=16&lt;BR /&gt;spidev spi1.0: Failed to setup transfer, error = -22&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;- Aditya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Sep 2016 02:39:48 GMT</pubDate>
    <dc:creator>adityapatil</dc:creator>
    <dc:date>2016-09-13T02:39:48Z</dc:date>
    <item>
      <title>imx283 spidev</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx283-spidev/m-p/611245#M92265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with imx283 and linux-2.6.35.3&lt;/P&gt;&lt;P&gt;Does the spidev support 16-bits transfer per word ?&lt;/P&gt;&lt;P&gt;I am able to use 8-bits per word.&lt;/P&gt;&lt;P&gt;But, if i set the bits to 16. Getting following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Output:&lt;/P&gt;&lt;P&gt;spidev spi1.0: mxs_spi_setup_transfer, unsupported bits_per_word=16&lt;BR /&gt;spidev spi1.0: Failed to setup transfer, error = -22&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;- Aditya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 02:39:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx283-spidev/m-p/611245#M92265</guid>
      <dc:creator>adityapatil</dc:creator>
      <dc:date>2016-09-13T02:39:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx283 spidev</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx283-spidev/m-p/611246#M92266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aditya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems driver in ..drivers/spi/spi_mxs.c mxs_spi_setup_transfer()&lt;/P&gt;&lt;P&gt;sets its mode as 8-bits per word, refer to attached Linux Manual&lt;/P&gt;&lt;P&gt;Chapter 21 SPI Bus Driver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 05:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx283-spidev/m-p/611246#M92266</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-13T05:20:43Z</dc:date>
    </item>
  </channel>
</rss>