<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx Krogoth Yocto patch /init.d/bluetooth help! in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-Krogoth-Yocto-patch-init-d-bluetooth-help/m-p/611092#M92241</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes in the end I did.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 06:38:54 GMT</pubDate>
    <dc:creator>edwardtyrrell</dc:creator>
    <dc:date>2017-02-22T06:38:54Z</dc:date>
    <item>
      <title>imx Krogoth Yocto patch /init.d/bluetooth help!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-Krogoth-Yocto-patch-init-d-bluetooth-help/m-p/611090#M92239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm after a few instructions on how to apply a custom patch to /etc/init.d/bluetooth within one of my own custom meta-layers.&lt;/P&gt;&lt;P&gt;With other patches/file updates I've done it's simply a matter of coping a like mannered path to my own layer to that of the one I need to change - e.g update a pulseaudio file I'd do =&amp;gt; meta-mylayer/recipes-multimedia/pulseaudio/etc, .&amp;nbsp; adding a bbappend and so. But how can I update /etc/init.d/bluetooth as it's not specifically in the sources/meta-....?&lt;/P&gt;&lt;P&gt;What would I have to include recipe wise inside my custom layer and how would the append work to apply a patch ( or replace the file out-right )? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thanks.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 16:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-Krogoth-Yocto-patch-init-d-bluetooth-help/m-p/611090#M92239</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2017-02-07T16:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx Krogoth Yocto patch /init.d/bluetooth help!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-Krogoth-Yocto-patch-init-d-bluetooth-help/m-p/611091#M92240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Edward Tyrrell,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you made progress on this regard?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a document which shows how to add a file, which you may use to replace the file altogether. You may then create a new image recipe or append on your new layer to include this recipe.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-105374"&gt;https://community.nxp.com/docs/DOC-105374&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is definitely not straightforward but I hope it helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Feb 2017 22:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-Krogoth-Yocto-patch-init-d-bluetooth-help/m-p/611091#M92240</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-02-21T22:02:38Z</dc:date>
    </item>
    <item>
      <title>Re: imx Krogoth Yocto patch /init.d/bluetooth help!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-Krogoth-Yocto-patch-init-d-bluetooth-help/m-p/611092#M92241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes in the end I did.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 06:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-Krogoth-Yocto-patch-init-d-bluetooth-help/m-p/611092#M92241</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2017-02-22T06:38:54Z</dc:date>
    </item>
  </channel>
</rss>