<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic android6.0 support camera flash in hal in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android6-0-support-camera-flash-in-hal/m-p/610954#M92223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the android6.0 system, the current debugging mipi camera ov5640 flash, but open the camera application,&amp;nbsp;there is &amp;nbsp;no flash options. How to open this option, such as flash on,&amp;nbsp;flash off ,etc.When I&amp;nbsp;use android4.3,I added the following code in the HAL layer, " &amp;nbsp;&amp;nbsp; &amp;nbsp; uint8_t flashAvailable = 1; &amp;nbsp; ADD_OR_SIZE(ANDROID_FLASH_INFO_AVAILABLE, &amp;amp;flashAvailable, 1); " camera flash option will appear in camera application auto.when i use android6.0, I also use Android4.3 method, but open the camera application&amp;nbsp;,there is not camera flash option, I would like to ask how to&amp;nbsp;modify the Android6.0 HAL layer to&amp;nbsp;let it support the flash option by default?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Mar 2017 02:30:36 GMT</pubDate>
    <dc:creator>yangguang</dc:creator>
    <dc:date>2017-03-02T02:30:36Z</dc:date>
    <item>
      <title>android6.0 support camera flash in hal</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android6-0-support-camera-flash-in-hal/m-p/610954#M92223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the android6.0 system, the current debugging mipi camera ov5640 flash, but open the camera application,&amp;nbsp;there is &amp;nbsp;no flash options. How to open this option, such as flash on,&amp;nbsp;flash off ,etc.When I&amp;nbsp;use android4.3,I added the following code in the HAL layer, " &amp;nbsp;&amp;nbsp; &amp;nbsp; uint8_t flashAvailable = 1; &amp;nbsp; ADD_OR_SIZE(ANDROID_FLASH_INFO_AVAILABLE, &amp;amp;flashAvailable, 1); " camera flash option will appear in camera application auto.when i use android6.0, I also use Android4.3 method, but open the camera application&amp;nbsp;,there is not camera flash option, I would like to ask how to&amp;nbsp;modify the Android6.0 HAL layer to&amp;nbsp;let it support the flash option by default?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 02:30:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android6-0-support-camera-flash-in-hal/m-p/610954#M92223</guid>
      <dc:creator>yangguang</dc:creator>
      <dc:date>2017-03-02T02:30:36Z</dc:date>
    </item>
  </channel>
</rss>