<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Yocto doesn't support git binary diff - workaround? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-doesn-t-support-git-binary-diff-workaround/m-p/610666#M92155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm making minor modifications to my Yocto project using a layer that includes git patch files called up by bbappend files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was working fine until I tried to add a new logo BMP file which causes git to produce a binary diff.&lt;/P&gt;&lt;P&gt;This cause bitbake to fail with:&lt;/P&gt;&lt;P&gt;File tools/logos/mx6ullevk.bmp: git binary diffs are not supported.&lt;BR /&gt;Patch 0002-First-steps-at-a-useable-python-file-to-create-bitma.patch does not apply (enforce with -f)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's a pain. Can someone suggest a simple work around?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.30.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "Ubuntu-16.04"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx6ull14x14evk"&lt;BR /&gt;DISTRO = "fsl-imx-fb"&lt;BR /&gt;DISTRO_VERSION = "4.1.15-2.0.1"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Mar 2017 16:41:10 GMT</pubDate>
    <dc:creator>chris_f</dc:creator>
    <dc:date>2017-03-22T16:41:10Z</dc:date>
    <item>
      <title>Yocto doesn't support git binary diff - workaround?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-doesn-t-support-git-binary-diff-workaround/m-p/610666#M92155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm making minor modifications to my Yocto project using a layer that includes git patch files called up by bbappend files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was working fine until I tried to add a new logo BMP file which causes git to produce a binary diff.&lt;/P&gt;&lt;P&gt;This cause bitbake to fail with:&lt;/P&gt;&lt;P&gt;File tools/logos/mx6ullevk.bmp: git binary diffs are not supported.&lt;BR /&gt;Patch 0002-First-steps-at-a-useable-python-file-to-create-bitma.patch does not apply (enforce with -f)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's a pain. Can someone suggest a simple work around?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.30.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "Ubuntu-16.04"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx6ull14x14evk"&lt;BR /&gt;DISTRO = "fsl-imx-fb"&lt;BR /&gt;DISTRO_VERSION = "4.1.15-2.0.1"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 16:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-doesn-t-support-git-binary-diff-workaround/m-p/610666#M92155</guid>
      <dc:creator>chris_f</dc:creator>
      <dc:date>2017-03-22T16:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto doesn't support git binary diff - workaround?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-doesn-t-support-git-binary-diff-workaround/m-p/610667#M92156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I worked around the problem by storing my new bmp in base64 encoded format and using the Makefile to produce the binary. It's not nice but it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 18:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-doesn-t-support-git-binary-diff-workaround/m-p/610667#M92156</guid>
      <dc:creator>chris_f</dc:creator>
      <dc:date>2017-03-22T18:06:03Z</dc:date>
    </item>
  </channel>
</rss>