<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSerial Downloader USB HID serial number</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610656#M92150</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi together,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using serial downloader in an i.MX7 device. When i look at the USB HID descriptor the serial number string is empty. Is there any way to get a serial number in serial downloader so that we can find the correct device if more than one is connected to the host?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Nov 2016 10:14:44 GMT</pubDate>
    <dc:creator>MA1979</dc:creator>
    <dc:date>2016-11-21T10:14:44Z</dc:date>
    <item>
      <title>Serial Downloader USB HID serial number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610656#M92150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi together,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using serial downloader in an i.MX7 device. When i look at the USB HID descriptor the serial number string is empty. Is there any way to get a serial number in serial downloader so that we can find the correct device if more than one is connected to the host?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 10:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610656#M92150</guid>
      <dc:creator>MA1979</dc:creator>
      <dc:date>2016-11-21T10:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Downloader USB HID serial number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610657#M92151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not 100% sure on this, but I assume you mean a way to program a USB PID and VID code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so then there are areas in the fuse map assigned for this, see the reference manual -&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9454i8BF3AE8788F614BC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are intended for customer use, what I'm not sure about is if there is a direct link between these fuse values and the serial loader mode, but I think it is likely, you can try programming a test value to see if it works as required, but for production I think you would need to be using registered VID and PID codes with the usb.org.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ross&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 18:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610657#M92151</guid>
      <dc:creator>RossMcLuckie</dc:creator>
      <dc:date>2016-11-21T18:55:57Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Downloader USB HID serial number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610658#M92152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Parameters, provided by i.MX7 boot ROM for USB boot loader, may be &lt;BR /&gt;found in section 6.6.9.1 (USB) of the i.MX7 Reference Manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;In Your case, perhaps the following helps, but this is OS dependent.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="" href="https://msdn.microsoft.com/en-us/library/ff539683.aspx" title="https://msdn.microsoft.com/en-us/library/ff539683.aspx"&gt;HidD_GetSerialNumberString routine (Windows Drivers)&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct &lt;BR /&gt;Answer button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 02:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610658#M92152</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-11-22T02:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Downloader USB HID serial number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610659#M92153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i don't want to programm VID or PID. I would like to porgramm a serial number which can be read by a function such as &lt;A class="" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fmsdn.microsoft.com%2Fen-us%2Flibrary%2Fff539683.aspx" rel="nofollow" target="_blank"&gt;HidD_GetSerialNumberString routine (Windows Drivers)&lt;/A&gt;. Currently the answer is empty on every device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 12:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610659#M92153</guid>
      <dc:creator>MA1979</dc:creator>
      <dc:date>2016-11-28T12:37:30Z</dc:date>
    </item>
    <item>
      <title>Re: Serial Downloader USB HID serial number</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610660#M92154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Boot ROM cannot be changed (programmed).&lt;/P&gt;&lt;P&gt;Perhaps, it makes sense to use USB addresses, which&lt;/P&gt;&lt;P&gt;are assigned &amp;nbsp;during enumeration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Dec 2016 04:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Serial-Downloader-USB-HID-serial-number/m-p/610660#M92154</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-12-02T04:09:41Z</dc:date>
    </item>
  </channel>
</rss>