<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX6 GPIO CONTROL PROBLEM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-CONTROL-PROBLEM/m-p/610629#M92148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have problem with GPIO pin on Board sabre SDP. When I export by SYSF pin EIM_DA0 I can't change value of this pin but when I export pin EIM_D18 I can change value without problem(I checked on osciloscope). I didn't see in device tree any configuration of that both pin but one work(EIM_D18) &amp;nbsp;and &amp;nbsp;EIM_DA0 doesn't. Do I need export pin to DeviceTree when I want use it as GPIO in SYSFS? Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Mar 2017 16:06:16 GMT</pubDate>
    <dc:creator>sebastianpszczo</dc:creator>
    <dc:date>2017-03-22T16:06:16Z</dc:date>
    <item>
      <title>IMX6 GPIO CONTROL PROBLEM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-CONTROL-PROBLEM/m-p/610629#M92148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have problem with GPIO pin on Board sabre SDP. When I export by SYSF pin EIM_DA0 I can't change value of this pin but when I export pin EIM_D18 I can change value without problem(I checked on osciloscope). I didn't see in device tree any configuration of that both pin but one work(EIM_D18) &amp;nbsp;and &amp;nbsp;EIM_DA0 doesn't. Do I need export pin to DeviceTree when I want use it as GPIO in SYSFS? Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 16:06:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-CONTROL-PROBLEM/m-p/610629#M92148</guid>
      <dc:creator>sebastianpszczo</dc:creator>
      <dc:date>2017-03-22T16:06:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 GPIO CONTROL PROBLEM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-CONTROL-PROBLEM/m-p/610630#M92149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello bb,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yes, you need to add it to device tree and multiplex it as GPIO.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 01:35:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-GPIO-CONTROL-PROBLEM/m-p/610630#M92149</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2017-03-23T01:35:58Z</dc:date>
    </item>
  </channel>
</rss>