<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX6 Java optimizations in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Java-optimizations/m-p/610608#M92143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are developing Java8 software in a Linux-on-iMX6 environment and we have read a quite old post &lt;A href="https://community.nxp.com/docs/DOC-1478"&gt;All Boards Java&lt;/A&gt;‌ about the advantages of using "Oracle Java SE Embedded" over the iMX* architectures.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are currently using "Oracle Java SE 8 for ARM" (&lt;STRONG&gt;not&lt;/STRONG&gt; the SE Embedded) with good outcomes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following the afore mentioned post we have made some tests with the SE Embedded 8 version for ARMv7, keeping&amp;nbsp;the same Java program on the same hardware, but we haven't noticed any relevant improvement&amp;nbsp;in the performances: are we missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We haven't re-compiled the Java program, we just changed the JVM: may this be the mistake? Should we use a special Java compiler to leverage any optimization of the iMX architecture?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We didn't find any clear explanation on this topic on the Internet, that's why we are writing here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Roberto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jan 2017 12:01:01 GMT</pubDate>
    <dc:creator>robertopierpaol</dc:creator>
    <dc:date>2017-01-12T12:01:01Z</dc:date>
    <item>
      <title>iMX6 Java optimizations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Java-optimizations/m-p/610608#M92143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are developing Java8 software in a Linux-on-iMX6 environment and we have read a quite old post &lt;A href="https://community.nxp.com/docs/DOC-1478"&gt;All Boards Java&lt;/A&gt;‌ about the advantages of using "Oracle Java SE Embedded" over the iMX* architectures.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are currently using "Oracle Java SE 8 for ARM" (&lt;STRONG&gt;not&lt;/STRONG&gt; the SE Embedded) with good outcomes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following the afore mentioned post we have made some tests with the SE Embedded 8 version for ARMv7, keeping&amp;nbsp;the same Java program on the same hardware, but we haven't noticed any relevant improvement&amp;nbsp;in the performances: are we missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We haven't re-compiled the Java program, we just changed the JVM: may this be the mistake? Should we use a special Java compiler to leverage any optimization of the iMX architecture?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We didn't find any clear explanation on this topic on the Internet, that's why we are writing here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Roberto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 12:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Java-optimizations/m-p/610608#M92143</guid>
      <dc:creator>robertopierpaol</dc:creator>
      <dc:date>2017-01-12T12:01:01Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Java optimizations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Java-optimizations/m-p/610609#M92144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; The example of the&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-1478"&gt;https://community.nxp.com/docs/DOC-1478&lt;/A&gt;&amp;nbsp; is relatively simple, hardly &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;great optimization may be gotten here. &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Also, note, it is needed to use hardware accelerators in software &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;for optimization, but standard Oracle VM for ARM is applied in the case.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please apply to Oracle for implementation details.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 06:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Java-optimizations/m-p/610609#M92144</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2017-01-16T06:09:39Z</dc:date>
    </item>
  </channel>
</rss>