<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Customization of U-Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Customization-of-U-Boot/m-p/609849#M91980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aditya Nagal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You do need to customize u-boot &amp;nbsp;and the device tree so that they reflect the hardware on your board.&lt;/P&gt;&lt;P&gt;My recommendation would be taking a configuration that’s close to your board and making the necessary changes. You can find a guide on customizing the device tree on the following community document:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-329664"&gt;https://community.nxp.com/docs/DOC-329664&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please consult the i.MX BSP Porting Guide which is available as part of the BSP Releases documentation for more information on how to port the BSP to your custom board including the bootloader.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Mar 2017 22:01:17 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-03-01T22:01:17Z</dc:date>
    <item>
      <title>Customization of U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customization-of-U-Boot/m-p/609848#M91979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;We need to bring-up the newly designed board .I have the folllowing questions: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Do we need to customized the U-boot , as per the board design or the standard u-boot which works on Reference boards will also work on the new board .&lt;/P&gt;&lt;P&gt;2. How to generate the device Tree binaries for the newly designed target board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aditya Nagal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Mar 2017 12:20:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customization-of-U-Boot/m-p/609848#M91979</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2017-03-01T12:20:50Z</dc:date>
    </item>
    <item>
      <title>Re: Customization of U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Customization-of-U-Boot/m-p/609849#M91980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aditya Nagal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You do need to customize u-boot &amp;nbsp;and the device tree so that they reflect the hardware on your board.&lt;/P&gt;&lt;P&gt;My recommendation would be taking a configuration that’s close to your board and making the necessary changes. You can find a guide on customizing the device tree on the following community document:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-329664"&gt;https://community.nxp.com/docs/DOC-329664&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please consult the i.MX BSP Porting Guide which is available as part of the BSP Releases documentation for more information on how to port the BSP to your custom board including the bootloader.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I hope this information helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Mar 2017 22:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Customization-of-U-Boot/m-p/609849#M91980</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-03-01T22:01:17Z</dc:date>
    </item>
  </channel>
</rss>