<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow to get output from mfgtool command line interface?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-get-output-from-mfgtool-command-line-interface/m-p/609551#M91911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using mfgTool2 from the command line with the -noui parameter. It downloads the firmware fine but there is no output in the cmd window. I am using this in a production environment in a C# program. I would like to be able to display the kinds of progress you see when mfgTool2 is run as a GUI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Oct 2016 13:52:06 GMT</pubDate>
    <dc:creator>raymatlin</dc:creator>
    <dc:date>2016-10-27T13:52:06Z</dc:date>
    <item>
      <title>How to get output from mfgtool command line interface?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-get-output-from-mfgtool-command-line-interface/m-p/609551#M91911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using mfgTool2 from the command line with the -noui parameter. It downloads the firmware fine but there is no output in the cmd window. I am using this in a production environment in a C# program. I would like to be able to display the kinds of progress you see when mfgTool2 is run as a GUI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2016 13:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-get-output-from-mfgtool-command-line-interface/m-p/609551#M91911</guid>
      <dc:creator>raymatlin</dc:creator>
      <dc:date>2016-10-27T13:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to get output from mfgtool command line interface?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-get-output-from-mfgtool-command-line-interface/m-p/609552#M91912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ray&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;available options are described in Quick Start Guide p.8, also one&lt;/P&gt;&lt;P&gt;can customize for own needs using sources&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools" title="https://github.com/NXPmicro/mfgtools"&gt;GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2016 09:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-get-output-from-mfgtool-command-line-interface/m-p/609552#M91912</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-28T09:03:20Z</dc:date>
    </item>
  </channel>
</rss>