<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX7 eLCD data assignment. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eLCD-data-assignment/m-p/609387#M91897</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;the i.MX7 eLCDIF provides flexible options for color_bits-to-pins mapping.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please take a look at section 13.2.4.2 (Write Data Path) of the i.MX7D Reference&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Manual for details regarding pixel data from frame buffer to LCD path. Data of&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;the frame buffer will be mapped to external LCD bus pins. In particularly,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;"WORD_LENGTH=3 indicates that the input frame-buffer is RGB 24 bits per pixel&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(RGB 888). If BYTE_PACKING_FORMAT [3:0] is 0x7, it indicates that there is only&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;one pixel per 32-bit word".&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;For example, for MCIMX28LCD display board :&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD00 Blue 0 (LSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD07 Blue 7 (MSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD08 Green 0 (LSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD15 Green 7 (MSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD16 Red 0 (LSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD23 Red 7 (MSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Sep 2016 07:14:37 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-09-14T07:14:37Z</dc:date>
    <item>
      <title>i.MX7 eLCD data assignment.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eLCD-data-assignment/m-p/609386#M91896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our customer have a question about i.MX7 eLCD.&lt;BR /&gt;Please see Table 13-4 in IMX7DRM Rev.0, they uderstand what pads should they use.&lt;BR /&gt;Howver, in Table 13-4, no data assigment is written, so they did not understand the connection between i.MX7 and LCD.&lt;BR /&gt;Would you let me know the data assignment?&lt;BR /&gt;(e.g. for RGB666, R[5:0]=LCD_D[17:12] G[5:0]=LCD_D[11:6] B[5:0]=LCD_D[5:0] with 18-bit DOTCLK LCD IF mode)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 09:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eLCD-data-assignment/m-p/609386#M91896</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2016-09-12T09:20:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 eLCD data assignment.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eLCD-data-assignment/m-p/609387#M91897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;the i.MX7 eLCDIF provides flexible options for color_bits-to-pins mapping.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please take a look at section 13.2.4.2 (Write Data Path) of the i.MX7D Reference&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Manual for details regarding pixel data from frame buffer to LCD path. Data of&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;the frame buffer will be mapped to external LCD bus pins. In particularly,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;"WORD_LENGTH=3 indicates that the input frame-buffer is RGB 24 bits per pixel&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(RGB 888). If BYTE_PACKING_FORMAT [3:0] is 0x7, it indicates that there is only&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;one pixel per 32-bit word".&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;For example, for MCIMX28LCD display board :&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD00 Blue 0 (LSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD07 Blue 7 (MSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD08 Green 0 (LSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD15 Green 7 (MSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD16 Red 0 (LSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LCD23 Red 7 (MSB)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 07:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-eLCD-data-assignment/m-p/609387#M91897</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-09-14T07:14:37Z</dc:date>
    </item>
  </channel>
</rss>