<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUsing the QuadSPI Flash on i.MX7 SABRE SDB</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-QuadSPI-Flash-on-i-MX7-SABRE-SDB/m-p/609034#M91867</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The NXP i.MX7 SABRE SDB has a on QSPI flash memory. &amp;nbsp;The schematic shows a MX25L51245GZ2I-10G device is populated. The schematic also indicates moving/removing some resistors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition to the resistor changes and SW2 Boot Config setting, are there instructions for programming and erasing the on-board QuadSPI flash memory device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At minimum, I would like to download a U-Boot image to the flash memory, so I can at least boot the SABRE SDB and load a Linux OS over a Ethernet network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dawei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 11 Sep 2016 19:41:05 GMT</pubDate>
    <dc:creator>daweichen</dc:creator>
    <dc:date>2016-09-11T19:41:05Z</dc:date>
    <item>
      <title>Using the QuadSPI Flash on i.MX7 SABRE SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-QuadSPI-Flash-on-i-MX7-SABRE-SDB/m-p/609034#M91867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The NXP i.MX7 SABRE SDB has a on QSPI flash memory. &amp;nbsp;The schematic shows a MX25L51245GZ2I-10G device is populated. The schematic also indicates moving/removing some resistors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition to the resistor changes and SW2 Boot Config setting, are there instructions for programming and erasing the on-board QuadSPI flash memory device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At minimum, I would like to download a U-Boot image to the flash memory, so I can at least boot the SABRE SDB and load a Linux OS over a Ethernet network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dawei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Sep 2016 19:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-QuadSPI-Flash-on-i-MX7-SABRE-SDB/m-p/609034#M91867</guid>
      <dc:creator>daweichen</dc:creator>
      <dc:date>2016-09-11T19:41:05Z</dc:date>
    </item>
    <item>
      <title>Re: Using the QuadSPI Flash on i.MX7 SABRE SDB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-QuadSPI-Flash-on-i-MX7-SABRE-SDB/m-p/609035#M91868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dawei&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for programming qspi please use MFG Tool and script&lt;BR /&gt;mfgtool2-yocto-mx-sabresd-qspi-nor-mx25l51245g.vbs, check documentation inside package&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Programmers (Flash, etc.) (2)&lt;BR /&gt;IMX6_L4.1.15_1.2.0_MFG_TOOL (REV L4.1.15_1.2.0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can use Demo Files:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recommended Software &amp;amp; Tools (5)&lt;BR /&gt;&amp;nbsp;L4.1.15_1.2.0_iMX7D (REV L4.1.15_1.2.0)&lt;BR /&gt;i.MX 7Dual SABRESD Linux Binary Demo Files&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Fsabre-development-system%2Fsabre-board-for-smart-devices-based-on-the-i.mx-7dual-applications-processors%3ARDIMX7DSABREBRD%3Ffpsp%3D1%26tab%3DDesign_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-7dual-applications-processors:RDIMX7DSABREBRD?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Recommended reading (pay attention to i.MX_Linux_User's_Guide.pdf included in L4.1.15_1.2.0_LINUX_DOCS):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Users Guides (1) &lt;BR /&gt;SABRE SDB for i.MX 7Dual - Quick Start Guide&lt;BR /&gt;Supporting Information (4) &lt;BR /&gt;L4.1.15_1.2.0_LINUX_DOCS&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Fsabre-development-system%2Fsabre-board-for-smart-devices-based-on-the-i.mx-7dual-applications-processors%3ARDIMX7DSABREBRD%3Ffpsp%3D1%26tab%3DDocumentation_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-7dual-applications-processors:RDIMX7DSABREBRD?fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;BR /&gt;Getting Started&lt;BR /&gt;&lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-7dual-applications-processors:RDIMX7DSABREBRD?tab=In-Depth_Tab"&gt;http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-board-for-smart-devices-based-on-the-i.mx-7dual-applications-processors:RDIMX7DSABREBRD?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Sep 2016 23:48:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-QuadSPI-Flash-on-i-MX7-SABRE-SDB/m-p/609035#M91868</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-11T23:48:42Z</dc:date>
    </item>
  </channel>
</rss>