<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Uboot Documentation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608989#M91857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor for the pointers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. While trying to capture the differences between DDR on Sabre board and our custom board, it seems to me that the delta between the two boards is larger than I had thought.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sabre board uses LPDDR3 MT41K128M16JT, whereas our custom board uses LPDDR2 EDB8164B4PT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. It also seems to me that in addition to applying changes to DCD file, I will also have to apply changes elsewhere too. Do you think I have understood it correctly or am I missing out on something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. Is there some other reference board from Freescale that uses the same processor as that on SabreDL, but interfaces to LPDDR2 chip? I can possibly use source code for that u-boot as a reference to customise for our board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Oct 2016 21:36:48 GMT</pubDate>
    <dc:creator>shani</dc:creator>
    <dc:date>2016-10-07T21:36:48Z</dc:date>
    <item>
      <title>Uboot Documentation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608986#M91854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.MX6 in our custom design. Our design is based on Sabre platform (&lt;A class="link-titled" href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT" title="http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/sabre-platform-for-smart-devices-based-on-the-i.mx-6-series:RDIMX6SABREPLAT"&gt;SABRE Platform for Smart Devices|NXP&lt;/A&gt;). Our software platform is going to be embedded linux. Both iMX6 and embedded linux are new technologies for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to find documentation for the bootloader (u-boot). I did try to search on NXP community website but am still a bit clueless. Could someone please provide links/pointers to u-boot documentation? In particular, I need to change the source code related to DDR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 17:13:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608986#M91854</guid>
      <dc:creator>shani</dc:creator>
      <dc:date>2016-10-05T17:13:07Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot Documentation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608987#M91855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In particular, I need to modify the DDR driver built into uboot for our custom platform, so any pointers on where to locate the current DDR source code in uboot and how/where to apply the changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2016 17:19:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608987#M91855</guid>
      <dc:creator>shani</dc:creator>
      <dc:date>2016-10-05T17:19:21Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot Documentation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608988#M91856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shani&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;changes should be entered to *.cfg file located in folder uboot/board/freescale/mx6sabresd&lt;/P&gt;&lt;P&gt;documentation is included in uboot/doc folder or one can check web version&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.denx.de/wiki/U-Boot/Documentation" title="http://www.denx.de/wiki/U-Boot/Documentation"&gt;Documentation &amp;lt; U-Boot &amp;lt; DENX&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2016 00:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608988#M91856</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-06T00:11:27Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot Documentation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608989#M91857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor for the pointers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. While trying to capture the differences between DDR on Sabre board and our custom board, it seems to me that the delta between the two boards is larger than I had thought.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sabre board uses LPDDR3 MT41K128M16JT, whereas our custom board uses LPDDR2 EDB8164B4PT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. It also seems to me that in addition to applying changes to DCD file, I will also have to apply changes elsewhere too. Do you think I have understood it correctly or am I missing out on something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. Is there some other reference board from Freescale that uses the same processor as that on SabreDL, but interfaces to LPDDR2 chip? I can possibly use source code for that u-boot as a reference to customise for our board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any thoughts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 21:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608989#M91857</guid>
      <dc:creator>shani</dc:creator>
      <dc:date>2016-10-07T21:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot Documentation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608990#M91858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shani&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/docs/DOC-94790"&gt;https://community.freescale.com/docs/DOC-94790&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?tab=Documentation_Tab&amp;amp;pspll=1&amp;amp;SelectedAsset=Documentation&amp;amp;ProdMetaId=PID/DC/QWKS-SCM-IMX6DQ&amp;amp;fromPSP=true&amp;amp;assetLockedForNavigation=true&amp;amp;componentId=2&amp;amp;leftNavCode=1&amp;amp;pageSize=25&amp;amp;Documentation=Documentation/00210KscRcb%60%60Application%20Notes&amp;amp;fpsp=1&amp;amp;linkline=Application%20Notes" title="http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?tab=Documentation_Tab&amp;amp;pspll=1&amp;amp;SelectedAsset=Documentation&amp;amp;ProdMetaId=PID/DC/QWKS-SCM-IMX6DQ&amp;amp;fromPSP=true&amp;amp;assetLockedForNavigation=true&amp;amp;componentId=2&amp;amp;leftNavCode=1&amp;amp;pageSize=25&amp;amp;Documentation=Documentation/00210KscRcb%60%60Application%20Notes&amp;amp;fpsp=1&amp;amp;linkline=Application%20Notes"&gt;Quick Start Board for SCM-i.MX 6DQ|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 23:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-Documentation/m-p/608990#M91858</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-10-07T23:59:21Z</dc:date>
    </item>
  </channel>
</rss>