<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック30Mbit/s clocked serial interface</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/30Mbit-s-clocked-serial-interface/m-p/608963#M91850</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a proprietary data connection to/from a data acquisition system that produces a NRZ encoded serial data stream of max 30Mbit/s. The connection shall be bi-directional.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What interface can be best used to receive this data in the iMX6? Would SPI be an option? Or are there better options?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your suggestions!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jan 2017 12:36:36 GMT</pubDate>
    <dc:creator>frankambrosius</dc:creator>
    <dc:date>2017-01-11T12:36:36Z</dc:date>
    <item>
      <title>30Mbit/s clocked serial interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/30Mbit-s-clocked-serial-interface/m-p/608963#M91850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a proprietary data connection to/from a data acquisition system that produces a NRZ encoded serial data stream of max 30Mbit/s. The connection shall be bi-directional.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What interface can be best used to receive this data in the iMX6? Would SPI be an option? Or are there better options?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your suggestions!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 12:36:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/30Mbit-s-clocked-serial-interface/m-p/608963#M91850</guid>
      <dc:creator>frankambrosius</dc:creator>
      <dc:date>2017-01-11T12:36:36Z</dc:date>
    </item>
    <item>
      <title>Re: 30Mbit/s clocked serial interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/30Mbit-s-clocked-serial-interface/m-p/608964#M91851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could take a look at the application note AN3020 “Configuring and Using the SPI”:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN3020.pdf"&gt;http://www.nxp.com/assets/documents/data/en/application-notes/AN3020.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regarding the specific information of the i.MX6 processor, you could refer to Table 51 “ECSPI Master Mode Timing Parameters” of i.MX 6Dual/6Quad Datasheet:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf"&gt;http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 Jan 2017 03:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/30Mbit-s-clocked-serial-interface/m-p/608964#M91851</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2017-01-15T03:08:44Z</dc:date>
    </item>
  </channel>
</rss>