<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.mx6plus mmdc profiler: AXI IDs, AXI ID MASK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6plus-mmdc-profiler-AXI-IDs-AXI-ID-MASK/m-p/608929#M91843</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you try to buld fsl-image-machine-test, please refer to attached Yocto Guide&lt;/P&gt;&lt;P&gt;Table 1 use build configurations for imx6qpsabreauto or imx6qpsabresd board&lt;/P&gt;&lt;P&gt;and add imx-test (folder ..test/mmdc has profile test) without source changes&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/Freescale/meta-fsl-arm/tree/master/recipes-bsp/imx-test" title="https://github.com/Freescale/meta-fsl-arm/tree/master/recipes-bsp/imx-test"&gt;meta-fsl-arm/recipes-bsp/imx-test at master · Freescale/meta-fsl-arm · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Sep 2016 23:47:14 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-09-12T23:47:14Z</dc:date>
    <item>
      <title>i.mx6plus mmdc profiler: AXI IDs, AXI ID MASK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6plus-mmdc-profiler-AXI-IDs-AXI-ID-MASK/m-p/608928#M91842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm migrating from i.mx6quad to i.mx6quad plus. In the imx6q I used the MMDC profiler to measure the load of the IPU0/1, GPU3D, VPU and the ARM cpus.&lt;/P&gt;&lt;P&gt;For the imx6qplus some of the AXI IDs have changed and the PRE0:3 was added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made the following changes to my profiling program:&lt;/P&gt;&lt;P&gt;ARM_S0/S1: no change&lt;/P&gt;&lt;P&gt;IPU1/2: no change&lt;/P&gt;&lt;P&gt;GPU3D0/1: from ID 2/3 to ID 6/E, mask unchanged&lt;/P&gt;&lt;P&gt;VPU: from ID 13 to 2, mask unchanged&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(based on the Applications Processor Reference Manual Rev 0, 02/2016)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The program used to report useful numbers for the i.mx6, with the changes above all counters stay at zero except when profiling the ARM cpu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are the AXI IDs and masks correct?&lt;/P&gt;&lt;P&gt;Is there anything else that has changed for the MMDC profiler?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Lo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Sep 2016 21:07:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6plus-mmdc-profiler-AXI-IDs-AXI-ID-MASK/m-p/608928#M91842</guid>
      <dc:creator>lotharfelten</dc:creator>
      <dc:date>2016-09-10T21:07:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6plus mmdc profiler: AXI IDs, AXI ID MASK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6plus-mmdc-profiler-AXI-IDs-AXI-ID-MASK/m-p/608929#M91843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you try to buld fsl-image-machine-test, please refer to attached Yocto Guide&lt;/P&gt;&lt;P&gt;Table 1 use build configurations for imx6qpsabreauto or imx6qpsabresd board&lt;/P&gt;&lt;P&gt;and add imx-test (folder ..test/mmdc has profile test) without source changes&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/Freescale/meta-fsl-arm/tree/master/recipes-bsp/imx-test" title="https://github.com/Freescale/meta-fsl-arm/tree/master/recipes-bsp/imx-test"&gt;meta-fsl-arm/recipes-bsp/imx-test at master · Freescale/meta-fsl-arm · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Sep 2016 23:47:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6plus-mmdc-profiler-AXI-IDs-AXI-ID-MASK/m-p/608929#M91843</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-09-12T23:47:14Z</dc:date>
    </item>
  </channel>
</rss>