<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Boot from eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608634#M91764</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please answer yes or no.&lt;/P&gt;&lt;P&gt;The problem of booting from eMMC is BOOT_CFG4[7]=1 " Infinite Loop Enable at start of boot ROM. Used for debugging purposes", i.e. it MUST be '0'. Right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 07:38:14 GMT</pubDate>
    <dc:creator>victormazhbits</dc:creator>
    <dc:date>2016-12-14T07:38:14Z</dc:date>
    <item>
      <title>Boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608632#M91762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'd like to verify a resistor's board setting to BOOT from eMMC (please see attached).&lt;/P&gt;&lt;P&gt;1) In my design because of board spacing issue i have put only pull-down resistors on EIM_DA0-DA15 (BOOT_CFG1[0-5,7],BOOT_CFG2[0-2,5-7,11-12] )&amp;nbsp;,i.e.&amp;nbsp;only '0' may be configured externally and '1' i 'trust' in internal pull-up.. i.e. i.MX6 reads a values of inputs approximatelly 300uS-1mS after reset released, so pulled-up voltage is already stable.&lt;/P&gt;&lt;P&gt;2) In compare to &lt;STRONG&gt;SPF-27392 rev.C3.pdf &lt;/STRONG&gt;(&lt;SPAN style="color: black; font-size: 10pt;"&gt;SabreSD schematic p.21 &lt;/SPAN&gt;) , I don't refer to EIM_A16-A24 (BT_CFG3_[0-7],BT_CFG4_0), EIM_WAIT/EIM_LBA/EIM_EB0,1/EIM_RW/EIM_EB2,3 (BT_CFG4_[1-7]).&lt;/P&gt;&lt;P&gt;Let's say that eMMC is already programmed.&lt;/P&gt;&lt;P&gt;I don't see any response on eMMC clock after power-up.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Actually in Manufacture Mode i can read write eMMC content.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advice.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 16:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608632#M91762</guid>
      <dc:creator>victormazhbits</dc:creator>
      <dc:date>2016-12-13T16:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608633#M91763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EIM_EB3 is floating, means BOOT_CFG4[7]=1 and&lt;/P&gt;&lt;P&gt;Infinite Loop Enable at of boot ROM. Used for debugging purposes.&lt;/P&gt;&lt;P&gt;This is described in Table 8-2. Boot eFUSE Descriptions&lt;/P&gt;&lt;P&gt;i.MX6DQ Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 00:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608633#M91763</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-14T00:39:35Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608634#M91764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please answer yes or no.&lt;/P&gt;&lt;P&gt;The problem of booting from eMMC is BOOT_CFG4[7]=1 " Infinite Loop Enable at start of boot ROM. Used for debugging purposes", i.e. it MUST be '0'. Right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 07:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608634#M91764</guid>
      <dc:creator>victormazhbits</dc:creator>
      <dc:date>2016-12-14T07:38:14Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608635#M91765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;it MUST be '0'. Right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 07:41:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608635#M91765</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-14T07:41:15Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608636#M91766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But, on the other hand, when i tried blow fuses (eMMC boot source) with &amp;nbsp;BOOT_CFG4[7]=0 (reset value)&amp;nbsp;-&amp;nbsp;it's still doesn't work...&lt;/P&gt;&lt;P&gt;May be you have an idea why?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW - eMMC was programmed not with &lt;STRONG&gt;".. &lt;SPAN style="color: black; font-size: 10pt;"&gt;MFG Tools for programming eMMC, run mfgtool2-yocto-mx-sabresd-emmc.vbs script, its ucl2.xml contains commands which uses that script. &lt;/SPAN&gt;&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;Is it critical?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thnk you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 14:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608636#M91766</guid>
      <dc:creator>victormazhbits</dc:creator>
      <dc:date>2016-12-14T14:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608637#M91767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;BTW - eMMC was programmed not with &lt;STRONG&gt;".. &lt;SPAN style="color: black; font-size: 10pt;"&gt;MFG Tools for programming eMMC, run &lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: black; font-size: 10pt;"&gt;&amp;gt;mfgtool2-yocto-mx-sabresd-emmc.vbs script, its ucl2.xml contains commands which uses that script. &lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;&amp;gt;Is it critical?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right this also may be reason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 00:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-from-eMMC/m-p/608637#M91767</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-12-15T00:51:08Z</dc:date>
    </item>
  </channel>
</rss>