<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Capacitor on input pin</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Capacitor-on-input-pin/m-p/608477#M91758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dirk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I doubt if placing capacitor on digital pin will produce good filtering,&lt;/P&gt;&lt;P&gt;"bouncing" may be caused by slow signal change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Feb 2017 23:22:24 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-02-28T23:22:24Z</dc:date>
    <item>
      <title>Capacitor on input pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capacitor-on-input-pin/m-p/608476#M91757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I connect the collector of an opto-coupler, ACPL-847-300E, with one PIN of the iMX6, PIN configured as GPIO inport, Schmitt-trigger, slow, 22kOhm. That works fine, inverted logic.&lt;/P&gt;&lt;P&gt;Now I placed a 3.3nF capacitor to that PIN, hoping to control the frequency, 1/2*PI*R*C, by the PIN control register.&lt;/P&gt;&lt;P&gt;But the behavior is not like expected. Falling edges lead to one edge, but rising edges lead to more then one rising-falling edge. Like the signal bounces around the threshold of being 1 or 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The put the filter in the entrance of the opto-coupler is more likley, I think. But the possibility to change the cutoff frequency would be nice.&lt;/P&gt;&lt;P&gt;Is it impossible, or would I need more then a capacitor?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 14:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capacitor-on-input-pin/m-p/608476#M91757</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2017-02-28T14:26:53Z</dc:date>
    </item>
    <item>
      <title>Re: Capacitor on input pin</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Capacitor-on-input-pin/m-p/608477#M91758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dirk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I doubt if placing capacitor on digital pin will produce good filtering,&lt;/P&gt;&lt;P&gt;"bouncing" may be caused by slow signal change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 23:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Capacitor-on-input-pin/m-p/608477#M91758</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-02-28T23:22:24Z</dc:date>
    </item>
  </channel>
</rss>