<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q，ADV7481，Can't get CSI data issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608190#M91729</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for reply. &amp;nbsp;:smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'v read the documents above, and make some changes at kernel level, just as "Sample code for iMX6 SabreSD to use MIPI CSI ca... | NXP Community" described.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the issue is not closed.It seems invalid.&lt;/P&gt;&lt;P&gt;With the mipi regs debug infos i memtioned above, the STATE reg is 0x300, and the ERR reg is 0x00, seems like mipi works well.&lt;/P&gt;&lt;P&gt;Now i want to print ome the ipu's regs info to get the status of ipu-modulle. How can i achieve it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Nov 2016 09:56:19 GMT</pubDate>
    <dc:creator>maninwind</dc:creator>
    <dc:date>2016-11-21T09:56:19Z</dc:date>
    <item>
      <title>IMX6Q，ADV7481，Can't get CSI data issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608188#M91727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i'm beginner of linux, working on imx6q platform, linux kernel is 3.14.28.&lt;/P&gt;&lt;P&gt;For now, i'm geting stuck in&amp;nbsp;debugging on adv7481，which connects to imx6q with mipi interface.&lt;/P&gt;&lt;P&gt;My problem looks&amp;nbsp;like "IPU can't get the CSI data". I choose the default ipu&amp;amp;csi setting, ipu0-csi1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i use "cat /dev/video0" command, following error log shows up:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;-&amp;gt; "ERROR: v4l2 capture: mxc_v4l_read timeout counter 0"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;-&amp;gt; "imx-ipu3 2400000.ipu: Not a CSI channel"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;-&amp;gt; "cat: read error: Timer expired"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i use "gst-launch-1.0 /dev/video1" command, following error log shows up:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;-&amp;gt; "ERROR: unrecognized std! 0 (PAL=ff, NTSC=b000"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;-&amp;gt; "(gst-launch-1.0:599): GStreamer-CRITICAL **: gst_element_make_from_uri: assertion 'gst_uri_is_valid (uri)' failed&lt;BR /&gt;ERROR: pipeline could not be constructed: no source element for URI "/dev/video1"."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is some&amp;nbsp;configs and settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In device tree , i cancel&amp;nbsp;the following configs, those has no relationship with debugging adv7481 i thought:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;1) lcd&amp;amp;backlight&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;2) v4l2_cap_0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;3) mipi_dsi_reset&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;4) pinctrl_ipu1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;5) pinctrl_ipu1_2(parallel camera setting)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I check the same problem in community, and modify the kernel souce with "0001-Correct-mipi-camera-virtual-channel-setting-in.patch".&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I print out the mipi.info para, and mipi regs, it seems like mipi working fine:&lt;/P&gt;&lt;P&gt;====Below is MipiInfo para ====&amp;gt;&lt;BR /&gt;mipi_csi2_info.mipi_en = 1&lt;BR /&gt;mipi_csi2_info.ipu_id = 0&lt;BR /&gt;mipi_csi2_info.csi_id = 1&lt;BR /&gt;mipi_csi2_info.v_channel = 0&lt;BR /&gt;mipi_csi2_info.lanes = 2&lt;BR /&gt;mipi_csi2_info.datatype = 30&lt;BR /&gt;&amp;lt;====Above is MipiInfo para ====&lt;BR /&gt;adv748x_mipi 1-0070: &lt;BR /&gt;====Below is MipiCsi2Regs para ====&amp;gt;&lt;BR /&gt;MIPI_CSI_N_LANES = 0x1&lt;BR /&gt;MIPI_CSI_PHY_SHUTDOWNZ = 0x1&lt;BR /&gt;MIPI_CSI_DPHY_RSTZ = 0x1&lt;BR /&gt;MIPI_CSI_CSI2_RESETN = 0x1&lt;BR /&gt;MIPI_CSI_PHY_STATE = 0x300&lt;BR /&gt;MIPI_CSI_DATA_IDS_1 = 0x0&lt;BR /&gt;MIPI_CSI_DATGA_IDS_2 = 0x0&lt;BR /&gt;MIPI_CSI_ERR1 = 0x0&lt;BR /&gt;MIPI_CSI_ERR2 = 0x0&lt;BR /&gt;&amp;lt;====Above is MipiCsi2Regs para ====&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know the reason here, is there something missing?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot. : )&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 03:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608188#M91727</guid>
      <dc:creator>maninwind</dc:creator>
      <dc:date>2016-11-21T03:06:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q，ADV7481，Can't get CSI data issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608189#M91728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can start configuring clocks using Debug steps for customer MIPI sensor.docx on&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fdocs%2FDOC-94312" rel="nofollow" target="_blank"&gt;https://community.freescale.com/docs/DOC-94312&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://community.freescale.com/docs/DOC-102233" title="https://community.freescale.com/docs/DOC-102233"&gt;Sample code for iMX6 SabreSD to use MIPI CSI ca... | NXP Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and appnote AN5305&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/assets/documents/data/en/application-notes/AN5305.pdf" title="http://www.nxp.com/assets/documents/data/en/application-notes/AN5305.pdf"&gt;http://www.nxp.com/assets/documents/data/en/application-notes/AN5305.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 05:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608189#M91728</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-11-21T05:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q，ADV7481，Can't get CSI data issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608190#M91729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for reply. &amp;nbsp;:smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'v read the documents above, and make some changes at kernel level, just as "Sample code for iMX6 SabreSD to use MIPI CSI ca... | NXP Community" described.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the issue is not closed.It seems invalid.&lt;/P&gt;&lt;P&gt;With the mipi regs debug infos i memtioned above, the STATE reg is 0x300, and the ERR reg is 0x00, seems like mipi works well.&lt;/P&gt;&lt;P&gt;Now i want to print ome the ipu's regs info to get the status of ipu-modulle. How can i achieve it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 09:56:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608190#M91729</guid>
      <dc:creator>maninwind</dc:creator>
      <dc:date>2016-11-21T09:56:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q，ADV7481，Can't get CSI data issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608191#M91730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue is fixed.&lt;/P&gt;&lt;P&gt;1) Make sure&amp;nbsp;the .dtsi file is right.&lt;/P&gt;&lt;P&gt;2) Make sure the driver of adv7481 is right.&lt;/P&gt;&lt;P&gt;3) No need to modify the 3.14.28 kernel.&lt;/P&gt;&lt;P&gt;4) Add the bootpara in U-Boot&lt;/P&gt;&lt;P&gt;5) Use "gst-launch-1.0 imxv4l2src device=/dev/videox ! imxv4l2sink" command test.&lt;/P&gt;&lt;P&gt;6) The video from HDMI Rx will display through HDMI Tx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 08:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-ADV7481-Can-t-get-CSI-data-issue/m-p/608191#M91730</guid>
      <dc:creator>maninwind</dc:creator>
      <dc:date>2016-11-29T08:18:51Z</dc:date>
    </item>
  </channel>
</rss>